STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Enable FDCAN_IT_ARB_PROTOCOL_ERROR

HelloI use CAN FD and have a functioning communication with 3 participants. Now I want to activate the interrupt that notifies me when the device has lost the arbitration contest. I forward each of the four NVIC interrupts in stm32h7xx_hal_fdcan: voi...

MFrie.7 by Associate III
  • 2632 Views
  • 5 replies
  • 0 kudos

STM32F4 having trouble into SLEEP mode

Posted on March 24, 2017 at 11:03Hello there,Currently I'm using a STM32F407VG discovery board to testing the stm32 low power features. STM32CubeMX was used to generate a simple demo. However, it seems always not able to enter sleep mode (standby mo...

stm32L562 error connection SWD

Hi! I have custom board with new mcu stm32l562ve. Board has out pins - SWDIO and SWCLK.I am try connect by st-link v3. But mcu not connected. Also, i tested with connect nRST ( setting "Under Reset" in st-link ). But this variant same as first. MCVU ...

dlpPavlo by Associate II
  • 2912 Views
  • 8 replies
  • 3 kudos

Resolved! STM32F407 VREF+ voltage not 3.3V

Hi, I have a custom board in which VREF+ is supposed to be 3.3V. But the actual VREF+ (pin32) is 2.xV, with drifts between power ups. VDDA (pin 33) is 3.3V.What's wrong with the circuit schematic? Can I just remove the resistor (R22) between VREF+ an...

stm32_vref.jpg
fzl by Associate II
  • 2461 Views
  • 5 replies
  • 1 kudos

Resolved! Blackpill and LIS3DH - issue with Sleep Mode.

When I use sleep mode while debug it sleep mode Works. But when I try runing code without using debug method it dosnot go in Sleep mode. When I chack current.When using debug method stape by stape.  Without using stape by stape debug method.Hear is t...

WhatsApp Image 2024-03-08 at 15.59.59_4747fd50.jpg WhatsApp Image 2024-03-08 at 15.59.59_c9f9cb4e.jpg
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.