STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32U545 Execution Speed Slower Than Expected

Software Environment:Windows platformConfigured using STM32CubeMXCompiled with STM32CubeIDEHardware Platform:NUCLEO-U545RE-QMCU: STM32U545 (Cortex-M33, ARMv8-M)Test Objective:We initially noticed slow SPI performance (CS low to CS high) and decided t...

xiangpu2001_0-1741297902502.png xiangpu2001_1-1741297902504.png xiangpu2001_2-1741297902505.png

DMA issue stop1

For my project I am using the LPUART on an STM32U545 and 585, currently I am using the normal GPDMA and this works like a charm in normal run mode. However I want to be in STOP1 and receive UART communication. As per the reference manual the GPDMA is...

mve_0-1744118025997.png mve_1-1744118043326.png
mve by Associate
  • 1141 Views
  • 1 replies
  • 2 kudos

memset() execution slower at some addresses

Hello,After some investigation was found that memset has different behavior executed from different places in flash. Data and instruction cache are off! Micro used is stm32h743xi.Function is called with following arguments --> memset(dummy, 0, 64)Its...

DApo.1 by Associate II
  • 8629 Views
  • 13 replies
  • 0 kudos

STM32 MCUs: load data to RAM and boot from there?

Hi,I'm aware of the BOOT0 pin which is available on most STM32 MCUs and allows to select the device being booted from Flash.Now my problem is, once shipped to an end user, this flash can't be updated easily. So it would be better to have a more simpl...

Resolved! Looking for MCU

Hello community,We are designing a low-cost pump controller and are looking for an MCU with the following specifications:MCU RequirementsFlash: 512 KBRAM: 128 KBGPIOs: 64 to 84Integrated RTCRTC cell supportNo wireless connectivity neededLowest possib...

parth4 by Associate II
  • 1788 Views
  • 4 replies
  • 3 kudos

STM32H7 MDMA With QSPI

Hi, I would like to use the MDMA with the QSPI on an STM32H743 or similar.I need to use the QSPI to interface with several multiplexed LCD displays and I want to use the QSPI in 'indirect' mode to send commands to the displays and DMA the pixel data ...

JF999 by Associate
  • 1790 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.