cancel
Showing results for 
Search instead for 
Did you mean: 

Blackpill and LIS3DH - issue with Sleep Mode.

Kai_Satone
Senior

When I use sleep mode while debug it sleep mode Works. But when I try runing code without using debug method it dosnot go in Sleep mode. When I chack current.

WhatsApp Image 2024-03-08 at 15.59.59_4747fd50.jpg

When using debug method stape by stape.

WhatsApp Image 2024-03-08 at 15.59.59_c9f9cb4e.jpg

 Without using stape by stape debug method.

Hear is the Code :-

#include "main.h"
#include "i2c.h"
#include "usart.h"
#include "gpio.h"
#include "string.h"
#include "stdio.h"
#include "math.h"
 
void SystemClock_Config(void);
 
 
#define LIS3DHTR_ADDR (0x1D)
 
/* LIS3DHTR registers */
#define LIS3DHTR_CTRL_REG1 0x20
#define LIS3DHTR_CTRL_REG4 0x23
#define LIS3DHTR_OUT_X_L   0x28
#define LIS3DHTR_INT1_CFG  0x30
#define LIS3DHTR_INT1_THS  0x32
#define LIS3DHTR_INT1_DURATION 0x33
#define LED_PIN GPIO_PIN_10
#define LED_GPIO_PORT GPIOA
 
#define FALL_THRESHOLD 24 // 24 mg
 
volatile uint8_t fallDetected = 0;
 
 
char *str={0};
uint8_t Rx_data;
 
 
 
 
int main(void)
{
  HAL_Init();
 SystemClock_Config();
 
  MX_GPIO_Init();
  MX_I2C1_Init();
  MX_USART2_UART_Init();
 
  HAL_UART_Receive_IT(&huart2, &Rx_data, 1);
 
      uint8_t ctrl_reg1_data = 0x27; // X, Y, Z axis enabled, power on mode, data rate selection = 10Hz
      HAL_I2C_Mem_Write(&hi2c1, LIS3DHTR_ADDR << 1, LIS3DHTR_CTRL_REG1, I2C_MEMADD_SIZE_8BIT, &ctrl_reg1_data, 1, HAL_MAX_DELAY);
 
      uint8_t ctrl_reg4_data = 0x00; // Continuous update, +/- 2g, Self-test disabled
      HAL_I2C_Mem_Write(&hi2c1, LIS3DHTR_ADDR << 1, LIS3DHTR_CTRL_REG4, I2C_MEMADD_SIZE_8BIT, &ctrl_reg4_data, 1, HAL_MAX_DELAY);
 
      uint8_t int1_cfg_data = 0x2A; // Enable interrupt on X, Y, Z axes' data overrun and data-ready events
      HAL_I2C_Mem_Write(&hi2c1, LIS3DHTR_ADDR << 1, LIS3DHTR_INT1_CFG, I2C_MEMADD_SIZE_8BIT, &int1_cfg_data, 1, HAL_MAX_DELAY);
 
      uint8_t int1_ths_data = FALL_THRESHOLD; // Set threshold for fall detection
      HAL_I2C_Mem_Write(&hi2c1, LIS3DHTR_ADDR << 1, LIS3DHTR_INT1_THS, I2C_MEMADD_SIZE_8BIT, &int1_ths_data, 1, HAL_MAX_DELAY);
 
      uint8_t int1_duration_data = 0x00; // Set duration of interrupt pulse to minimum value
      HAL_I2C_Mem_Write(&hi2c1, LIS3DHTR_ADDR << 1, LIS3DHTR_INT1_DURATION, I2C_MEMADD_SIZE_8BIT, &int1_duration_data, 1, HAL_MAX_DELAY);
 
  while (1)
  {
  HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, 0);
  HAL_Delay(5000);
  char str[100]; // Declare str at the beginning
  strcpy(str, "Going into SLEEP MODE in 5 seconds\r\n");
      HAL_UART_Transmit(&huart2, (uint8_t *)str, strlen (str), 100);
 
      HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, 1);
        HAL_Delay(10000);
      HAL_SuspendTick();
 
      HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, 0);  // Just to indicate that the sleep mode is activated
 
      HAL_PWR_EnableSleepOnExit ();
 
              char message="shreyash";
              uint8_t data[6]={0};
                      HAL_I2C_Mem_Read(&hi2c1, LIS3DHTR_ADDR << 1, LIS3DHTR_OUT_X_L | 0x80, I2C_MEMADD_SIZE_8BIT, data, 6, HAL_MAX_DELAY);
 
                      int16_t xAccl = ((int16_t)((data[1] << 8| data[0]));
                      int16_t yAccl = ((int16_t)((data[3] << 8| data[2]));
                      int16_t zAccl = ((int16_t)((data[5] << 8| data[4]));
 
 
      sprintf(str, "\r\nx: %d ,\r\ny: %d ,r\nz: %d\r\n", xAccl,yAccl,zAccl);
      HAL_UART_Transmit(&huart2, (uint8_t *)str, sizeof(str), 100);
 
      //char magnitude = sqrt(xAccl * xAccl + yAccl * yAccl + zAccl * zAccl);
      char magnitude = sqrt(pow(xAccl, 2) + pow(yAccl, 2) + pow(zAccl, 2));
      sprintf(str, " trupti  %d\r \n",(int)( magnitude/10));
      HAL_UART_Transmit(&huart2,(uint8_t *)str, sizeof(str), 100);
 
      if((magnitude/10)>=20)
        {
 
        }
          else{
 
 
          HAL_UART_Transmit(&huart2, "below\r\n", strlen ("below\r\n"), HAL_MAX_DELAY);
            }
 
 
        strcpy(str, "Going into SLEEP(below) MODE in 5 seconds\r\n");
            HAL_UART_Transmit(&huart2, (uint8_t *)str, strlen (str), 100);
 
            HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, 1);
              HAL_Delay(100);
 
            HAL_SuspendTick();
 
            HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, 0);  // Just to indicate that the sleep mode is activated
 
            HAL_PWR_EnableSleepOnExit ();
  }
}
 
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) {
    if (GPIO_Pin == GPIO_PIN_0)
    { // Change according to your setup
        HAL_PWR_DisableSleepOnExit();
 
        char *wake_msg = "WakeUP from SLEEP\r\n";
        HAL_UART_Transmit(&huart2, (uint8_t *)wake_msg, strlen(wake_msg), 1000);
 
        for (int i=0; i<5; i++)
    {
      HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_4);
 
       HAL_Delay(5000);
    }
 
 
        char str[100]; // Declare str at the beginning
          strcpy(str, "Going into SLEEP(above) MODE in 5 seconds\r\n");
              HAL_UART_Transmit(&huart2, (uint8_t *)str, strlen (str), 100);
 
              HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, 1);
                HAL_Delay(10000);
              HAL_SuspendTick();
 
              HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, 0);  // Just to indicate that the sleep mode is activated
 
              HAL_PWR_EnableSleepOnExit ();    }
}

 

 

Thank you

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

ST resources are dedicated to supporting genuine ST products. We are not committed to ensuring that clones/fakes work properly with the firmware we provide.

Thank you for your understanding.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Andrew Neil
Super User

Please use this button to properly post source code:

AndrewNeil_0-1709894959505.png

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
/* USER CODE BEGIN Header */
/**
  ******************************************************************************
  * @file           : main.c
  * @brief          : Main program body
  ******************************************************************************
  * @attention
  *
  * Copyright (c) 2024 STMicroelectronics.
  * All rights reserved.
  *
  * This software is licensed under terms that can be found in the LICENSE file
  * in the root directory of this software component.
  * If no LICENSE file comes with this software, it is provided AS-IS.
  *
  ******************************************************************************
  */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "i2c.h"
#include "usart.h"
#include "gpio.h"
#include "string.h"
#include "stdio.h"
#include "math.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */


#define LIS3DHTR_ADDR (0x1D)

/* LIS3DHTR registers */
#define LIS3DHTR_CTRL_REG1 0x20
#define LIS3DHTR_CTRL_REG4 0x23
#define LIS3DHTR_OUT_X_L   0x28
#define LIS3DHTR_INT1_CFG  0x30
#define LIS3DHTR_INT1_THS  0x32
#define LIS3DHTR_INT1_DURATION 0x33
#define LED_PIN GPIO_PIN_10
#define LED_GPIO_PORT GPIOA

/* Threshold for fall detection */
#define FALL_THRESHOLD 24 // 24 mg

volatile uint8_t fallDetected = 0;


char *str={0};
uint8_t Rx_data;




/* USER CODE END 0 */

/**
  * @brief  The application entry point.
  * @retval int
  */
int main(void)
{
  /* USER CODE BEGIN 1 */

  /* USER CODE END 1 */

  /* MCU Configuration--------------------------------------------------------*/

  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();

  /* USER CODE BEGIN Init */

  /* USER CODE END Init */

  /* Configure the system clock */
  SystemClock_Config();

  /* USER CODE BEGIN SysInit */

  /* USER CODE END SysInit */

  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_I2C1_Init();
  MX_USART2_UART_Init();
  /* USER CODE BEGIN 2 */
  HAL_UART_Receive_IT(&huart2, &Rx_data, 1);
  /* LIS3DHTR initialization */
      uint8_t ctrl_reg1_data = 0x27; // X, Y, Z axis enabled, power on mode, data rate selection = 10Hz
      HAL_I2C_Mem_Write(&hi2c1, LIS3DHTR_ADDR << 1, LIS3DHTR_CTRL_REG1, I2C_MEMADD_SIZE_8BIT, &ctrl_reg1_data, 1, HAL_MAX_DELAY);

      uint8_t ctrl_reg4_data = 0x00; // Continuous update, +/- 2g, Self-test disabled
      HAL_I2C_Mem_Write(&hi2c1, LIS3DHTR_ADDR << 1, LIS3DHTR_CTRL_REG4, I2C_MEMADD_SIZE_8BIT, &ctrl_reg4_data, 1, HAL_MAX_DELAY);

      uint8_t int1_cfg_data = 0x2A; // Enable interrupt on X, Y, Z axes' data overrun and data-ready events
      HAL_I2C_Mem_Write(&hi2c1, LIS3DHTR_ADDR << 1, LIS3DHTR_INT1_CFG, I2C_MEMADD_SIZE_8BIT, &int1_cfg_data, 1, HAL_MAX_DELAY);

      uint8_t int1_ths_data = FALL_THRESHOLD; // Set threshold for fall detection
      HAL_I2C_Mem_Write(&hi2c1, LIS3DHTR_ADDR << 1, LIS3DHTR_INT1_THS, I2C_MEMADD_SIZE_8BIT, &int1_ths_data, 1, HAL_MAX_DELAY);

      uint8_t int1_duration_data = 0x00; // Set duration of interrupt pulse to minimum value
      HAL_I2C_Mem_Write(&hi2c1, LIS3DHTR_ADDR << 1, LIS3DHTR_INT1_DURATION, I2C_MEMADD_SIZE_8BIT, &int1_duration_data, 1, HAL_MAX_DELAY);

  /* USER CODE END 2 */

  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {
    /* USER CODE END WHILE */
	  HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, 0);
	  HAL_Delay(5000);
	  char str[100]; // Declare str at the beginning
		  strcpy(str, "Going into SLEEP MODE in 5 seconds\r\n");
		    	  HAL_UART_Transmit(&huart2, (uint8_t *)str, strlen (str), 100);

		    	  HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, 1);
		      	  HAL_Delay(10000);
//	           EnterSleepMode();

		    /*    Suspend Tick increment to prevent wakeup by Systick interrupt.
		    	  Otherwise the Systick interrupt will wake up the device within 1ms (HAL time base)
		    */
		    	  HAL_SuspendTick();

		    	  HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, 0);  // Just to indicate that the sleep mode is activated

		    	  HAL_PWR_EnableSleepOnExit ();

		    	  	     	  char message="shreyash";
		    	  	 //    	   sprintf(str, "shreyash");
		    	  	 //    	   HAL_UART_Transmit(&huart2, str, sizeof(str), 100);

		    	  	     	  uint8_t data[6]={0};
		    	  	     	        	  HAL_I2C_Mem_Read(&hi2c1, LIS3DHTR_ADDR << 1, LIS3DHTR_OUT_X_L | 0x80, I2C_MEMADD_SIZE_8BIT, data, 6, HAL_MAX_DELAY);

		    	  	     	        	  int16_t xAccl = ((int16_t)((data[1] << 8) | data[0]));
		    	  	     	        	  int16_t yAccl = ((int16_t)((data[3] << 8) | data[2]));
		    	  	     	        	  int16_t zAccl = ((int16_t)((data[5] << 8) | data[4]));


		    	  	sprintf(str, "\r\nx: %d ,\r\ny: %d ,r\nz: %d\r\n", xAccl,yAccl,zAccl);
		    	  	HAL_UART_Transmit(&huart2, (uint8_t *)str, sizeof(str), 100);

		    	  	 //char magnitude = sqrt(xAccl * xAccl + yAccl * yAccl + zAccl * zAccl);
		    	  	 char magnitude = sqrt(pow(xAccl, 2) + pow(yAccl, 2) + pow(zAccl, 2));
		    	  	 sprintf(str, " trupti  %d\r \n",(int)( magnitude/10));
		    	  	 HAL_UART_Transmit(&huart2,(uint8_t *)str, sizeof(str), 100);

		    	  	if((magnitude/10)>=20)
		    	  	  {

		    	  		 HAL_GPIO_EXTI_Callback(GPIO_PIN_0);
//		    	  		 HAL_PWR_EnterSLEEPMode(PWR_MAINREGULATOR_ON, PWR_SLEEPENTRY_WFI);
//
//
//
//		    	  			    //	  Resume Tick interrupt if disabled prior to sleep mode entry
//		    	  			    	  HAL_ResumeTick();
//
//		    	  		//	    	  str = "WakeUP from SLEEP\r\n";
//		    	  			    	  HAL_UART_Transmit(&huart2, "WakeUP from SLEEP\r\n", strlen ("WakeUP from SLEEP\r\n"), HAL_MAX_DELAY);
//
//		    	  			    	  for (int i=0; i<5; i++)
//		    	  			    	  {
//		    	  			    		  HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_4);
//
//		    	  			    		  HAL_Delay(100);
//
//		    	  			    	  }
		    	  	  }
		    	  	    else{


		    	  	    	 HAL_UART_Transmit(&huart2, "below\r\n", strlen ("below\r\n"), HAL_MAX_DELAY);
		    	  	      }


		    	  			  strcpy(str, "Going into SLEEP(below) MODE in 5 seconds\r\n");
		    	  			    	  HAL_UART_Transmit(&huart2, (uint8_t *)str, strlen (str), 100);

		    	  			    	  HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, 1);
		    	  			      	  HAL_Delay(100);
		    	  	//	           EnterSleepMode();

		    	  			    /*    Suspend Tick increment to prevent wakeup by Systick interrupt.
		    	  			    	  Otherwise the Systick interrupt will wake up the device within 1ms (HAL time base)
		    	  			    */
		    	  			    	  HAL_SuspendTick();

		    	  			    	  HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, 0);  // Just to indicate that the sleep mode is activated

		    	  			    	  HAL_PWR_EnableSleepOnExit ();
    /* USER CODE BEGIN 3 */
  }
}

void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) {
    if (GPIO_Pin == GPIO_PIN_0)
    { // Change according to your setup
        HAL_PWR_DisableSleepOnExit();

        char *wake_msg = "WakeUP from SLEEP\r\n";
        HAL_UART_Transmit(&huart2, (uint8_t *)wake_msg, strlen(wake_msg), 1000);

        for (int i=0; i<5; i++)
    {
      	HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_4);

       HAL_Delay(5000);
    }


        char str[100]; // Declare str at the beginning
        		  strcpy(str, "Going into SLEEP(above) MODE in 5 seconds\r\n");
        		    	  HAL_UART_Transmit(&huart2, (uint8_t *)str, strlen (str), 100);

        		    	  HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, 1);
        		      	  HAL_Delay(10000);
        //	           EnterSleepMode();

        		    /*    Suspend Tick increment to prevent wakeup by Systick interrupt.
        		    	  Otherwise the Systick interrupt will wake up the device within 1ms (HAL time base)
        		    */
        		    	  HAL_SuspendTick();

        		    	  HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, 0);  // Just to indicate that the sleep mode is activated

        		    	  HAL_PWR_EnableSleepOnExit ();
        // Additional logic to handle wakeup event
    }
}

//void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin_4)
//{
//    str = "WakeUP from SLEEP by EXTI\r\n";
//    HAL_UART_Transmit(&huart2, (uint8_t *)str, strlen (str), HAL_MAX_DELAY);
//    HAL_PWR_DisableSleepOnExit ();
//}
  /* USER CODE END 3 */
//  void EnterSleepMode(void) {
//      // Indicate going to sleep
//      char *sleep_msg = "Going into SLEEP MODE\r\n";
//      HAL_UART_Transmit(&huart2, (uint8_t *)sleep_msg, strlen(sleep_msg), 1000);
//      HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, 1);
//       HAL_Delay(10000);
//      HAL_SuspendTick();
//      HAL_PWR_EnterSLEEPMode(PWR_MAINREGULATOR_ON, PWR_SLEEPENTRY_WFI);
//      HAL_ResumeTick();
//  }



/**
  * @brief System Clock Configuration
  * @retval None
  */
void SystemClock_Config(void)
{
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

  /** Configure the main internal regulator output voltage
  */
  __HAL_RCC_PWR_CLK_ENABLE();
  __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

  /** Initializes the RCC Oscillators according to the specified parameters
  * in the RCC_OscInitTypeDef structure.
  */
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
  RCC_OscInitStruct.HSEState = RCC_HSE_ON;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
  RCC_OscInitStruct.PLL.PLLM = 12;
  RCC_OscInitStruct.PLL.PLLN = 96;
  RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
  RCC_OscInitStruct.PLL.PLLQ = 4;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }

  /** Initializes the CPU, AHB and APB buses clocks
  */
  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)
  {
    Error_Handler();
  }
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
  * @brief  This function is executed in case of error occurrence.
  * @retval None
  */
void Error_Handler(void)
{
  /* USER CODE BEGIN Error_Handler_Debug */
  /* User can add his own implementation to report the HAL error return state */
  __disable_irq();
  while (1)
  {
  }
  /* USER CODE END Error_Handler_Debug */
}

#ifdef  USE_FULL_ASSERT
/**
  * @brief  Reports the name of the source file and the source line number
  *         where the assert_param error has occurred.
  * @PAram  file: pointer to the source file name
  * @PAram  line: assert_param error line source number
  * @retval None
  */
void assert_failed(uint8_t *file, uint32_t line)
{
  /* USER CODE BEGIN 6 */
  /* User can add his own implementation to report the file name and line number,
     ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
  /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
mƎALLEm
ST Employee

Hello,

ST resources are dedicated to supporting genuine ST products. We are not committed to ensuring that clones/fakes work properly with the firmware we provide.

Thank you for your understanding.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.