STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Which PWR_WAKEUP_PIN was used to wake from STANDBY?

Hello,I'm working with the STM32L031K6T and I'm going to standby without RTC and waking up the MCU with the A0 or A2 without problems, but for the application I need to know which PWR_WAKEUP_PIN was used to wake it up. Its possible to get a flag afte...

APrud.1 by Associate II
  • 2831 Views
  • 6 replies
  • 0 kudos

How to configure FDCAN1 with multiple RX filters?

I am using STM32G4 which allows 28 standard ID filters and 8 extended ID filters. This is from the Classic Frame Networking example:/* Configure Rx filter */ FDCAN_FilterTypeDef sFilterConfig;   sFilterConfig.IdType = FDCAN_STANDARD_ID; sFilter...

DLin.3 by Associate II
  • 1322 Views
  • 0 replies
  • 0 kudos

Resolved! Challeng with I2C1 and I2C2

Hello, I am working with a costumer board using STM32F105. There are some LED drivers working I2C1 and I2c2. Configuration for serial interfaces is:void MX_I2C1_Init(void){ /* USER CODE BEGIN I2C1_Init 0 */ /* USER CODE END I2C1_Init 0 */ /* USER COD...

NASI by Senior
  • 2350 Views
  • 4 replies
  • 0 kudos

Resolved! How fast can SPI run on a Nucleo board?

Hi all, I'm developing our application which requires high speed SPI. Currently I'm using the Nucleo-G070 for development and my peripheral device is connected to the Nucleo SPI pins with 6" jumper wires.I was trying to see what clock the peripheral ...

Konami by Senior II
  • 8325 Views
  • 3 replies
  • 0 kudos

Resolved! Unable to use USART1 to output in serial on STM32H7B3I-DK

I am having trouble trying to output data via USART1 on my STM32H7B3I-DK. According to the doc (UM2569), USART1 is a virtual com port connected to the USB STLINK (CN14). So I should theoretically be able to use USART1 to output to my serial console v...

JTurn.2 by Senior
  • 2077 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.