2021-10-12 8:11 AM
I am having trouble trying to output data via USART1 on my STM32H7B3I-DK. According to the doc (UM2569), USART1 is a virtual com port connected to the USB STLINK (CN14). So I should theoretically be able to use USART1 to output to my serial console via the Mirco-USB connected to my laptop? But for some reason my serial console isn't outputting anything at all. I have already checked that the settings for USART1 in STM32CubeMX and serial console match, so I am assuming it has nothing to do with my serial console's settings.
Here is a code snippet of my main loop and USART1. The code was essentially generated by STM32CubeMX after I selected the correct discovery board in 'board selector'.
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* Configure the peripherals common clocks */
PeriphCommonClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_FMC_Init();
MX_I2C1_Init();
MX_I2C4_Init();
MX_I2S6_Init();
MX_LTDC_Init();
MX_OCTOSPI1_Init();
MX_RTC_Init();
MX_SDMMC1_SD_Init();
MX_SPI1_Init();
MX_SPI2_Init();
MX_USART1_UART_Init();
MX_USART2_UART_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
uint8_t Test[] = "Hello World !!!\r\n"; //Data to send
HAL_UART_Transmit(&huart1,Test,sizeof(Test),10);// Sending in normal mode
HAL_Delay(1000);
}
/* USER CODE END 3 */
}
static void MX_USART1_UART_Init(void)
{
/* USER CODE BEGIN USART1_Init 0 */
/* USER CODE END USART1_Init 0 */
/* USER CODE BEGIN USART1_Init 1 */
/* USER CODE END USART1_Init 1 */
huart1.Instance = USART1;
huart1.Init.BaudRate = 115200;
huart1.Init.WordLength = UART_WORDLENGTH_8B;
huart1.Init.StopBits = UART_STOPBITS_1;
huart1.Init.Parity = UART_PARITY_NONE;
huart1.Init.Mode = UART_MODE_TX_RX;
huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart1.Init.OverSampling = UART_OVERSAMPLING_16;
huart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart1.Init.ClockPrescaler = UART_PRESCALER_DIV1;
huart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&huart1) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetTxFifoThreshold(&huart1, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetRxFifoThreshold(&huart1, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_DisableFifoMode(&huart1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN USART1_Init 2 */
/* USER CODE END USART1_Init 2 */
}Thank you for your help!
Solved! Go to Solution.
2021-10-12 9:54 AM
I see. Thank you for your advice. I used the debugger to step through my code and realised that there's an event handler error at 'MX_SDMMC1_SD_Init' which was stopping the rest of the code from running as I did not have a micro SD card inserted in my board. I managed to get a reading after adding an sd card to my board or by commenting out the event handler.
2021-10-12 8:59 AM
It's not necessary to like your own posts.
Check that it's not ending up in the Error_Handler() or other while loop, stop/check with a debugger.
Check RCC, GPIO and USART1 register settings.
Check define for HSE_VALUE, or clock from the HSI clock source.
2021-10-12 9:54 AM
I see. Thank you for your advice. I used the debugger to step through my code and realised that there's an event handler error at 'MX_SDMMC1_SD_Init' which was stopping the rest of the code from running as I did not have a micro SD card inserted in my board. I managed to get a reading after adding an sd card to my board or by commenting out the event handler.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.