logger application
any logger application for stm32 MCUs that use FAT on external flash is available ?thanks.
Ask questions, find answers, and share insights on STM32 products and their technical features.
any logger application for stm32 MCUs that use FAT on external flash is available ?thanks.
hi i have a problem with the F103 the adc reading is jumpy and all over the place too much noise while reading i tried to filter it by summing some and deviding by it but its still jumpy
Hello,I'm testing the SPI peripheral through a simple PDM mic. The problem is the SPI doesn't start at all. The CSTART bit (that is the one that start the transfer) remain cleared, even right after I SET the bit.Now, I noticed that just after I've do...
Hello, I design a device, based on STM32L475RE MCUand my goal is to minimize the power consumption.Peripheral I use :3 sensors(accelerometer, temperature, humidity) and external RTC(M41T64Q6F) on I2C busExternal flash on SPIUSBADC to read battery lev...
Does anyone can Help ?
Hello STM32 Family,Good AfternoonHope you are Safe and Happy.Currently we are working with STM32 Controllers, We have Received one New Task ..we are sharing Project code with our clients , How they can Edit the Code and Flash to controller without ha...
HelloTest Szenario: Transfer uint64_t counter from STM to another MC called ALFA.ALFA has a separate uint64_t counter.Each transfer counts the counter up.ALFA compares both counters and reports a missmatchSetup:ALFA -> SPI Master @ 10MhzSTMG4 -> SPI ...
I use STM32F429IGT6, Internal reset OFF, VBAT use external battery. offen reset error. datasheet tell me this configure is wrong. I want know what happen in internal stm32? Is RTC,backup SRAM,backup registers reset error or other?
Hi, My project goal to digitize a sine wave of frequency 20KHz and voltage varying from 0V to 3.3V using ADC of STM32H743ZI. I am using NUCLEO-H743ZI2.My doubt is how to choose ADC clock frequency so that I would be able to digitize the signal with...
In the datasheet (RM0444) for 512k dual bank devices, it looks like the last page of bank 1 is 127 and the first page of bank 2 is 256 (see section 3.3.1)The flash control register (see 3.7.5) says, the valid values for PNB is from 0 (page 0) to 0x17...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.