STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hardware problem with NSS pin on SPI

I cannot to set NSS pin in push-pull mode. What is may be wrong?I use SPI1 on stm32F7 as a master only mode with SSOE config bit. My system use SPI clock speed 13,5 MHz. GPIOA#4 is used as NSS pin alternative function 5, push-pull output.This configu...

0693W00000FC0s2QAD.bmp
Natsu by Associate II
  • 7581 Views
  • 7 replies
  • 0 kudos

How to use CD4094BE with 74HC595 shift registers

Hi Experts,I have a project like below. I am trying to send the data but the LEDS are not glowing in sending pattern.I am new to STM32F207 Nucleo board. Could anyone please let me know if I am missing anything.STM32f207 ======> CD4094(Q0) ==========>...

Bkris.2 by Associate II
  • 1634 Views
  • 0 replies
  • 0 kudos

Resolved! Current measurement with STM32L562QE-DK

Hello,I want to use the STM32L562QE-DK board to measure the current for my own developed PCBA. There is a connector CN20 that can be used for this purpose as written in the schematic for the board:Output connector to supply and measure external targe...

c_dev05 by Associate III
  • 1393 Views
  • 1 replies
  • 0 kudos

Hi, I'm trying to figure out why my basic timer interrupt on the STM32H7B3x dev board isn't working as expected. It seems to be triggering more often than I expect depending on when I clear the flag within the interrupt.

I am using the STM32H7B3LI-DK dev kit and want to use a simple timer with an interrupt. Using the most basic function, I've added a variable that simply increments within the interrupt. The timer is configured to hit the preloaded value at approx 1ms...

SThom.6 by Associate II
  • 4318 Views
  • 9 replies
  • 0 kudos

How to use function in main.c I want to make function about operate state. using interrupt! Plz check my main code. and check my error. Error[Pe065]: expected a ";

/* USER CODE END Header */   /* Includes ------------------------------------------------------------------*/   #include "main.h"   #include "usart.h"   #include "gpio.h"   #include "stm32h750xx.h"   #include "ESP32.h"   #include "stm32h7xx_hal_uart....

wwgww by Associate II
  • 2399 Views
  • 3 replies
  • 0 kudos

configure master/slaves timers on stm32f746

Hi, tell me, please. On stm32f746, tim3 is configured in encoder mode and works as a master for Timers 2,4,5,1,9. All Slave timers are in external clock mode 1, trigger source in accordance with the table:Tim2 - itr2Tim4 - itr2Tim5 - itr1Tim1- itr2Ti...

VKyri by Associate
  • 998 Views
  • 0 replies
  • 0 kudos

I want my STMF103RE based system to sit in Stop Mode and then wake up when a CAN message arrives, do something about it, and go back to Stop Mode.

 I want my system to sit in Stop Mode and then wake up and receive and process a CAN message when one arrives.     The code I generated for setting up the system includes: RCC->APB1ENR |= ( 1UL << 25);     /* enable clock for CAN -- Note: MCBSTM32 us...

HHeet.1 by Associate II
  • 3275 Views
  • 6 replies
  • 0 kudos

Resolved! STM32L496VET6

Hi There We need this stock STM32L496VET6. Please help us out,

UChan.2 by Associate
  • 1104 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.