STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32L471 Bootloader and SPI

Hello, I'm using STM32L471 and Micron MT25QL NOR Flash with single SPI interface. MT25 is also connected with other MCU (NRF52) using the same lines. I'm trying to write STM firmware in BOOT0 serial bootloader controlled by NRF using STM's USART3. Th...

Resolved! STM32L412 Wake from Low Power Sleep when Encoder is turned

Hi, what is the best way to wake from Low Power Sleep when an Encoder is rotated?I have TIM2 setup in encoder mode and it works when in Low Power Run. I just want to switch back from LP Sleep to LP Run when it's turned. Looking in stm32l4xx_hal_tim.c...

Lanceh by Associate III
  • 857 Views
  • 4 replies
  • 0 kudos

Resolved! STM32L4A6 and dual Bank (BFB2)

Hello,I'm having an issue with the STM32L4A6(1Mb) and the dual-bank.First of all, I tried with the NUCLEO-L476 and a simple blink led. It worked fine.Now, my project is based on a STM32L4A6, but the firmware doesn't start in BANK2.For simplicity, I d...

PCu1_0-1754304811567.png
PCu1 by Senior
  • 1024 Views
  • 4 replies
  • 0 kudos

STM32H747i-Disco Display

I am using an STM32H747i-Disco board for a time critical application. I would like to periodically output simple text messages to the display.but I don't want to use an RTOS, so TouchGFX is not an option. In LCD.c there appear to be no functions to s...

AStew.1 by Associate II
  • 672 Views
  • 3 replies
  • 1 kudos

Resolved! STM32 SPI Cant Set SSM Bit

Hi, Im new to STM32 and Im writing a bare metal spi library however for some reason when I try to change the SSM bit in code it doesnt seem to work. Im able to change the SSM bit in debug mode. void SPI_Enable(SPI_Com* spi) { SPI1_CLK_EN; //Reset...

Resolved! Board with STM32G0B1CEU6N microcontroller (MCU)

Hello All,I have received a PCB which is used in a battery pack that i am working on. Unfortunately the CM does not communicate any more and the last he told me was that they did not flash the devices. The PCB has basic functionalities like displayin...

Programming custom board STM32G0B1RET

Hi,I'm trying to program one custom board with STM32G0B1RET using original STLINK V3 and STLINK V2 without succes.My schematic is very simple as you can see on the image: And the response all time is: Not STM32 target found.. if I use SWD port. If I ...

micropap_0-1755374418337.png
micropap by Associate
  • 780 Views
  • 2 replies
  • 1 kudos

Resolved! stm32L476VE ADC reading opamp channel does not work

I have designed an L476 into a simple controller (BMS) and am trying to use the opamp and ADC and comparators to read the current, and implement a hardware fast overcurrent protection.The opamp is working fine in PGA mode G16. I can see as I inject 2...

DMolo_1-1755334809364.png DMolo_0-1755334775142.png DMolo_2-1755334820167.png DMolo_3-1755334894702.png
DMolo by Senior
  • 1717 Views
  • 6 replies
  • 0 kudos

Programming a virgin STM32G0B1

I'm trying to program a virgin SYM32G0B1 with the code I've developed and successfully run on the NUCLEO-G0B1RE/NUG0B1RE$AU2 development board. I'm using the STM32CibeProgrammer 2.20.0 software and an FTDI cable (TTL-232RG-VIP-WE with the Vcc line co...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.