STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Unable to sink 5V over USB PD

I am using an STM32G4 microcontroller with UCPD and the USBPD middleware. I was following this tutorial (same as AN5418 https://www.st.com/resource/en/application_note/dm00663511-how-to-build-a-simple-usbpd-sink-application-with-stm32cubemx-stmicroel...

Nv7_0-1742192885965.png
Nv7 by Associate III
  • 3246 Views
  • 10 replies
  • 0 kudos

Resolved! mt25ql512abb in memory mapped mode not working

I am writing a custom driver for the mt25ql512abb as the one on STM's github doesnt work for my STM32L412KB, I have gotten reading, writing and erasing working but when I try enter memory mapped mode DQ[0-3] on the flash just goes highHere is my func...

fhumphrys by Associate II
  • 1423 Views
  • 6 replies
  • 1 kudos

TIMER accuracy

Hello,I’m currently working on a project to synchronize two ICG and ECG devices. Although they require different oscillator frequencies—and therefore use different timers—both timers are driven by the same APB1 clock.Phase offsetSince they share the ...

welsonTW by Associate
  • 777 Views
  • 2 replies
  • 0 kudos

Resolved! STM32C0 DMAMUX SYNC example

Dear community,I would like to send a char buffer through UART using DMA, but at a precise interval (or delay).I know how to use the DMA with USART TX, it works flawlessly.The interesting bit is the delay between the DMA transfers.I know I can do it ...

Kraal by Lead
  • 2105 Views
  • 8 replies
  • 3 kudos

Resolved! Reference manual typo.

Hello,There's a small typo in the STM32H750VB reference manual (RM0433 Rev 8).Page 545, GPIO alternate function high register (GPIOx_AFRH)Address offset: 0x2 : Should be 0x24 (confirmed by the GPIO register map).Have a nice day, thanks for the very e...

Briztal by Associate
  • 2043 Views
  • 3 replies
  • 1 kudos

Nucleo-DRP1M1 with Nucleo-G0B1RE

Im currently facing issues with DRP1M1 and the Nucleo-G0B1RE in source configuration.I followed the instructions in the wiki however it seems that no actual communication is happening between the USB PD Devices this is the log i get from the cube mon...

PKrem.1 by Associate II
  • 814 Views
  • 3 replies
  • 0 kudos

Vbat minimum on STM32N6

I am designing the power system for an application using the STM32N645. In the datasheet for the STM32N6x5 minimum Vbat is defined as "TBD". In the STM32N6570-DK schematic the Vbat rail is set to 3.3V. If it can operate at 1.8V it would simplify the ...

Screenshot 2025-08-13 at 5.31.19 PM.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.