STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SDRAM MPU configuration for LTDC 1280x720

Hi, I have problem config LTDC for 1280x720 @60Hz. Without caching it works no problem, but slow. We are using 32MB SDRAM 16bit, config at 100MHz. When we use MPU to cache SDRAM, code as below: ``` MPU_Region_InitTypeDef MPU_InitStruct; /* Disable t...

Dat Tran by Senior II
  • 551 Views
  • 1 replies
  • 0 kudos

Resolved! FDCAN - DUAL ID FILTER

In this code I want IDs 0x100 and 0x200 should only be accepted but in my code all IDs are accepted. How to resolve this?/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file ...

STMUser_1 by Associate II
  • 2312 Views
  • 15 replies
  • 0 kudos

STM32H7S3L8 USB core reset timeout

Hey, we have purchased the Nucleo board H7S3L8-B02. We always run in a timeout during USB core reset. This problem seems quite popular with multiple forum posts. However we still didn't manage to get it to run. I will give a set by step explanation o...

USB_OTG_FS_setting.png CDC_setting.png PWR_USB_REG_setting.png USB_clock_setting.png
STesil by Associate
  • 949 Views
  • 2 replies
  • 0 kudos

Resolved! STM32 builtin bootloader GO command problem

Hi,I am trying to set up bootloader on my STM32G030, via usart. When I enter it and send start command (0x7F) I do get ACK response(0x79). I cna read ID and protocol verions, but when I try do use "Go" command to start my application, it gets stuck.W...

KlemenDS by Associate II
  • 2120 Views
  • 3 replies
  • 1 kudos

STM32U031F8P6 stop1 current

Hey all,I’m trying to squeeze the lowest possible STOP1 current out of an STM32U031F8P6 (TSSOP-20), no external crystals. The board itself looks fine: in the deepest mode (Shutdown/Standby) I see < 0.5 µA, so I don’t think it’s a hardware leak.Goal (...

Current graph.png
leddel32 by Associate II
  • 854 Views
  • 1 replies
  • 1 kudos

I can't read sdram framebuffer with LTDC

I am developping STM32F469 with TouchGFX to display with LTDC in RGB888. I can display an image in the internal SRAM. However, when trying with SDRAM, the screen truns black, and the debugger can only read 0s. But when I tried with the framebuffer re...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.