2025-08-30 8:45 AM
I am developping STM32F469 with TouchGFX to display with LTDC in RGB888. I can display an image in the internal SRAM. However, when trying with SDRAM, the screen truns black, and the debugger can only read 0s. But when I tried with the framebuffer reader offered by ST, I can still read the image which seems to be already loaded into the SDRAM. Is there any suggestions to figure out the issue to give a final solution?
2025-09-01 1:29 AM - edited 2025-09-01 1:29 AM
Hello @123scy321 and welcome to the community;
Could you please check the SDRAM configuration for that you can refer to How to set up the FMC peripheral to interface with the SDRAM IS42S16800F-6BLI from ISSI article.
Also, I recommend you to take a look at AN4861 application note precisely "5.5.2 Optimizing the LTDC framebuffer fetching from external memories (SDRAM or SRAM)" and "5.5.3 Optimizing the LTDC framebuffer fetching from SDRAM" sections.
I hope this help you!
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.