STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32N6 DK stuck when generate default project

Hi,Im just getting my new STM32N6570-DK and I try blinking simple led project first with default generate.But when I built and flash it, it got stuck when init UCPD (pic 1), am I missing something ?When I checking seem it still not define yet (pic 2)...

Micls_0-1756704854553.png Micls_1-1756704869910.png
Micls by Associate
  • 685 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F042K6 - USB Library too big for device?

 Hello everyone, I am using the STM32F042K6 for a small project where I don't have much space. Therefore, I rely on the small package and the "crystal-less USB" function. The hardware arrived today, but unfortunately, I had to realize that the USB li...

PP11 by Associate II
  • 4836 Views
  • 10 replies
  • 8 kudos

STM32G0 minimum ADC frequency

Hi,  I don't understand why CubeMX is limiting me through their IOC file to select an ADC clock below 2MHz. The datasheet says 140 kHz is the minimum ADC clock frequency for the STM32G07. Anyone has any answers or help ?. 

Resolved! Unable to execute code in SDRAM on STM32H745

Hi all,Board: STM32H745I-DISCOIDE: 1.16.1 I am facing some issues with trying to execute code on the SDRAM. I have a 2nd stage bootloader that loads the user application onto QSPI located at 0x9000 0000. After that, I copy the user application code t...

Resolved! Place constant at end of used flash - not specific address

Heyho,how can I put a constant at the end of the STM32's used flash? (using: STM32CubeIDE)Not at a specific address (that's not a problem), but I'd like to have a constant always at the end of the used internal flash, independent of any other source ...

LCE by Principal II
  • 2595 Views
  • 29 replies
  • 7 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.