2025-08-29 8:52 PM - last edited on 2025-09-01 3:09 AM by Andrew Neil
Hey everybody,
I was wondering if someone could help me correct my firmware that I've written.
I created a custom board using the STM32C011F4P6 MCU. I put an FTDI UART-to-USB converter on the board to be able to view outgoing messages from the custom board on my laptop.
While writing the firmware needed to demonstrate this functionality of the board, I referenced the C011 reference manual. There, STM describes the following steps to take when transmitting a character via USART, on page 752. I have tried to follow their advice to the best of my ability, but I notice that my board hangs while waiting for the transmission of a character to complete.
My testing code (in my main.c) is shown below:
int main(void)
{
char msg[] = "d";
// initialize debug LED
user_led_init();
// initialize the usart
usart_init();
while (1) {
// transmit string of characters (one character here)
usart_write_chars(msg, strlen(msg));
toggle_led();
delay_ms(500);
}
return 0;
}Here are the definitions of my usart_init and usart_write_chars functions:
// Author: Aidan Stanford
/* Writing a quick polling UART driver */
/* The main goal of this driver is to interface the STM32C011
* processor with the FTDI USB-to-UART converter on the breakout
* board.
* It is very bare bones. No interrupts or DMA stuff yet!
*/
// TODO: Organize header files better
#include <stdint.h>
#include "stm32c0xx.h"
#include "uart.h"
#include "main.h"
// This function modifies USART2->BRR
void usart_config_br(int baud)
{
// Do math according to the kernel clock source used
uint32_t div = (USART_APB_CLK / (USART_IND_PSC<<1) / baud);
// Set the BSRR register with the result from above
if (USART2->CR1 & (1U<<15)) // oversampling by 8
USART2->BRR = ((div & 0XFFF0) | ((div & 0XF) >> 1)) & ~(0X8);
else
USART2->BRR = div;
}
void usart_init(void)
{
/* Configure appropriate GPIOA pins */
// Enable GPIOA clocks!
RCC->IOPENR |= (RCC_GPIOA_CEN);
// Set speed to high
GPIOA->OSPEEDR |= GPIO_PA4_HS | GPIO_PA5_HS;
// Set pins PA5 and PA4 to AF mode and define their functions
GPIOA->MODER &= ~GPIOA_UART_MSK;
GPIOA->MODER |= GPIO_PA4_AF | GPIO_PA5_AF;
GPIOA->AFR[0] |= (GPIOA_USART2_AF<<16) | (GPIOA_USART2_AF<<20);
// Enable APB clock for USART2
RCC->APBENR1 |= RCC_USART2_CEN;
// Configure usart_ker_ck prescaler of 5 (ends up being 10)
USART2->PRESC |= USART_IND_PSC;
// configure baud rate
usart_config_br(9600);
// Enable the USART peripheral
USART2->CR1 |= USART_EN;
}
// Polling
void usart_read_chars(char *buf, int size)
{
}
void usart_write_chars(char *buf, int size)
{
int c = 0;
USART2->CR1 |= USART_TXE;
while (c < size) {
USART2->TDR = ((int)buf[c]) & 0XFF;
while (!(USART2->ISR & USART_TXE)) {}
++c;
}
/* This is where I hang */
while ((USART2->ISR & (1U<<6))) {}
}Any chance someone has developed with this MCU before and can give me a reality/sanity check on my code?
Thanks so much!
Solved! Go to Solution.
2025-08-30 6:57 AM
1)
while ((USART2->ISR & (1U<<6))) {}Supposing that you want to test USART_ISR_TC here, this test looks backwards, since once the Transmission Complete-s it will stay Complete.
2) Looking at RM0490 (r5) Sec 26.8.9, the protocol for using TC is more complex than this code expects -- you have to clear TC (via ISR:TCCF), and at just the right time to avoid a race. Unless you have a particular need (half-duplex single wire e.g.) I suggest you not do this at all: Just return from the function and let the USART do the final shift-out in the background.
3) You're using the same bit name (USART_TXE) in two different contexts. My best guess is that you're working with USART_ISR_TXE_TXFNF (bit 7) in one case and USART_CR1_TE (bit 3) in the other, so one of them is incorrect. The CMSIS naming conventions are designed to avoid this kind of conflict (at least it's highly visible); I suggest you stick with the CMSIS names.
2025-08-29 10:08 PM
Perhaps you could use the debugger, step the code, and check you've used the right bits.
Stick a scope on the pins, check the signals.
Perhaps just loop with the LED toggling, confirm that works.
Confirm board level functionality with HAL code.
2025-08-30 6:57 AM
1)
while ((USART2->ISR & (1U<<6))) {}Supposing that you want to test USART_ISR_TC here, this test looks backwards, since once the Transmission Complete-s it will stay Complete.
2) Looking at RM0490 (r5) Sec 26.8.9, the protocol for using TC is more complex than this code expects -- you have to clear TC (via ISR:TCCF), and at just the right time to avoid a race. Unless you have a particular need (half-duplex single wire e.g.) I suggest you not do this at all: Just return from the function and let the USART do the final shift-out in the background.
3) You're using the same bit name (USART_TXE) in two different contexts. My best guess is that you're working with USART_ISR_TXE_TXFNF (bit 7) in one case and USART_CR1_TE (bit 3) in the other, so one of them is incorrect. The CMSIS naming conventions are designed to avoid this kind of conflict (at least it's highly visible); I suggest you stick with the CMSIS names.
2025-08-30 7:53 AM - edited 2025-08-30 7:55 AM
Yes, the USART_TXE is likely problematic, it would make sense to enable USART_TE to the initialization. Double check the bit patterns.
The TC is an unnecessary wait, likely to stall into the ms realm, best just to wait on the buffer, which can fill while the active data is sent. Some of the newer STM32 models also have deeper FIFO, whereas the older one was much more shallow.
2025-09-01 6:45 AM
Hi bmckenney,
Great catch! Yes, I was mixing up the flags. I've now switched to using the flag naming conventions listed in the stm32c011.h header file. Not sure why I haven't been doing that sooner, my user header files are now a lot smaller!
My logic for checking the flag was also off, so I've fixed that as well.
However, I noticed that even after fixing these issues, I was still unable to get the board to print anything useful.
I then went back to Cube and made a HAL project to verify that I could print at all. I was able to get a clean "hello world\r\n" using Cube, so I knew then that something else was wrong with my code that I hadn't fixed yet. So I looked through the initialization functions generated by Cube, and I found that it did something very different than me:
huart2.Init.ClockPrescaler = UART_PRESCALER_DIV1;I had been setting the USART2->PRESC register to 5U in my original code, since I thought that it would work! And I was led to believe that it would by the times I had seen characters transmitted at the beginning of my problem (albeit they were in the wrong order), without framing errors or anything that I could see with the logic analyzer.
So after leaving the prescaler register at its default value (0), I was finally able to print hello world.
Thanks for all the help!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.