STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F302VCT6 - PC14 -> RTC_OUT_CALIB ?

I would like to set a 1Hz signal on the PC14 (RTC_OUT_CALIB). I have found a manual in document AN3371 (see picture in appendix). The code is also in the appendix. Unfortunately, nothing happens on the PC14 but the RTC works. If anyone has any idea w...

_legacyfs_online_stmicro_images_0693W00000dDc1sQAC.png
SimonFu by Associate
  • 429 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H7 DMA

HelloCan the STM32H743 modify data at two non-consecutive peripheral addresses in a single DMA event,A DMA event changes two peripheral addresses,

zhaowhong by Associate III
  • 529 Views
  • 1 replies
  • 0 kudos

Resolved! STM32N6 IMX219 camera

Hello,I'm trying to port the ST IMX335 camera driver middleware to work with the RPi 2 IMX219. Everything works well with the IMX335, however after adjusting to reflect the IMX219 registers I get no image data and a Lane 0& 1 control error flag as so...

Scheduling timers for motor control

Hi!I'm struggling to wrap my head around timers - I am trying to schedule some ADC reads of a current sense amplifier in a motor control setup.I have three center-aligned PWM waveforms being generated by Timer1, which successfully commutate a BLDC mo...

sb_st by Senior II
  • 730 Views
  • 3 replies
  • 0 kudos

Resolved! STM32G0: PWM Generation

I am using NUCLEO-G071RB. I am trying to generate an PWM pulse. I am using TIMER 3 Channel 2. - Clock Frequency = 64 MHzWith this setting I should get a HIGH pulse of 90 micro second, instead I get 80 or 40 micro seconds. When the Pre-scaler is incre...

jowakar122_0-1761917837043.png

USBX mic streaming on WBA65

Hello ST Community,I'm working on implementing USB Audio Class 2.0 with both speaker and microphone functionality on STM32WBA65 using USBX middleware.Request for Example: Are there any complete working examples of USBX Audio Class 2.0 with microphone...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.