STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

In Windows I can't see USBD Descriptors

 Hello there, I use USB CDC interface and I am sure that all my configurations are okey. There is no problem about connecting and data transfer between windows and my system, but there is a problem about descriptors such as "Manufacturer" or name of ...

Durukan by Associate
  • 1962 Views
  • 4 replies
  • 3 kudos

Resolved! Power Supply for STM32F030 Cortex TSSOP20 VDDA and VDD pin

Please i need help. The datasheet, says the VDDA voltage level must be always greater or equal to the VDD voltage leveland must be provided first. My qustion is: will my circuit work, if I tie the VDDA and VDD together, to be powered by the same  LDO...

fredy by Associate
  • 1112 Views
  • 5 replies
  • 3 kudos

Bare metal USART2 clock speed question

Hello,I am learning bare metal programming for STM32F446RE and am trying to write a simple transmit driver for USART2. I managed to do it but my only problem is when I use HSI 16Mhz clock speed (or anything lower) I get a weird first character. When ...

STMnoob_0-1758935979151.png
STMnoob by Associate II
  • 1280 Views
  • 6 replies
  • 2 kudos

Resolved! About FDCAN ERROR

Dear STM experts:     I am using the STM32G473RET6 chip for classic mode communication debugging in FDCAN, but there is a phenomenon where I cannot send information. In FDCAN-PSR, I can see an error of LEC being 5. After removing the CAN chip (SN65HV...

Resolved! SWD connection failed multiple times on STM32H725

We have a batch of custom boards using the STM32H725IGK3 and have experienced several failures getting started with them as the SWD interface appears to be fried. Initially we thought just bad luck with the first couple (inexperienced engineers or ?)...

niallp by Associate III
  • 1912 Views
  • 9 replies
  • 7 kudos

Resolved! GPIO input external pullup question

Testing a board with STM32U5A5. VDD is 3.3VI have configured one GPIO as input with an external pullup to 3.3V through a 470k ohm resistor.The input reads high, but when I measure the input with a scope, I read 2.2V on the input, which is below 0.7VD...

TLin.5 by Associate III
  • 1452 Views
  • 8 replies
  • 4 kudos

Resolved! Typo in the AN4660

Hello ST Community teamThe pin F11 on the TFBGA216 figure (figure 4 of the AN4660) should be VDD and not VSS according to the products datasheets (for the STM32F469N and STM32F769Nx6). That should be rectified on the next doc revision. Best Regards.I...

Issamos by Lead III
  • 560 Views
  • 1 replies
  • 2 kudos

Query about internal SMPS of STM32H757

I am trying to apply this configuration to my STM32H757 MCU where I am making a development board. here few things confuses me. 1. I have selected this configuration for better efficiency + noise performance. guide me if I am wrong2. What is the VDD ...

taj_0-1761655986257.png
taj by Associate II
  • 536 Views
  • 2 replies
  • 0 kudos

Resolved! STM32N6xxx SMPS internal , external

Hi Everybody1) There are some technical o specific reasons, that I was not able to find in the various documentations, to use external SMPS for VDDCORE insted of the internal one ?2) Working on NUCLEO-N675X0-Q, to configure various bridge for interna...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.