2025-11-02 5:52 PM
Hello
Can the STM32H743 modify data at two non-consecutive peripheral addresses in a single DMA event,A DMA event changes two peripheral addresses,
Solved! Go to Solution.
2025-11-02 11:23 PM
There are 4 DMAs in 'H743, of 3 types.
The MDMA probably could do this on its own, through scatter-gather, but the MDMA can be triggered only by "high-profile" peripherals such as JPEG, QUADSPI, DMA2D, LTDC.
The remaining DMAs are triggered through their respective DMAMUX. Directly, neither of these DMAs can transfer to non-consecutive addresses; however, there may be a trick (costing one extra DMA stream): the DMAMUX, together with triggering its own DMA stream (transferring to the first address) can generate an Event upon every transfer (see DMAMUX_CxCR.EGE), that in turn can be set as trigger for the Request generator in the DMAMUX, and that can generate a trigger (request) for a different DMAMUX channel triggering a different DMA stream, transferring to the second address.
JW
2025-11-02 11:23 PM
There are 4 DMAs in 'H743, of 3 types.
The MDMA probably could do this on its own, through scatter-gather, but the MDMA can be triggered only by "high-profile" peripherals such as JPEG, QUADSPI, DMA2D, LTDC.
The remaining DMAs are triggered through their respective DMAMUX. Directly, neither of these DMAs can transfer to non-consecutive addresses; however, there may be a trick (costing one extra DMA stream): the DMAMUX, together with triggering its own DMA stream (transferring to the first address) can generate an Event upon every transfer (see DMAMUX_CxCR.EGE), that in turn can be set as trigger for the Request generator in the DMAMUX, and that can generate a trigger (request) for a different DMAMUX channel triggering a different DMA stream, transferring to the second address.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.