2025-10-31 6:41 AM
I am using NUCLEO-G071RB. I am trying to generate an PWM pulse. I am using TIMER 3 Channel 2.
- Clock Frequency = 64 MHz
With this setting I should get a HIGH pulse of 90 micro second, instead I get 80 or 40 micro seconds. When the Pre-scaler is increased to 640-1, I received HIGH pulse of 980 and 920 micro second which was also not accurate.
Solved! Go to Solution.
2025-10-31 10:45 PM - edited 2025-10-31 11:31 PM
The issue is solved. My logic analyzer was capturing pulses at a low rate after increasing the rate I got the pulses.
2025-10-31 8:50 AM
hello @jowakar122
can you share your .ioc file please
BR
Gyessine
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-10-31 8:51 PM
2025-10-31 10:45 PM - edited 2025-10-31 11:31 PM
The issue is solved. My logic analyzer was capturing pulses at a low rate after increasing the rate I got the pulses.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.