STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! CRC calculation in STM32G4

Hi,I am working with STM32G491RE in my project. I have to transmit data through UART and I need to calculate CRC for that data.in my application:txdata[0] = 0x78;txdata[1] = 0x04;txdata[2] = 0x11;txdata[3] = 0x01; I have to calculate CRC16 for txdata...

STM32L4 power consumption reduction

Hi,I've created a PCB with an STM32L4x6 microcontroller and several peripherals, mainly I2C. I want to sample data at 512Hz using the internal ADC. The original plan was to configure the ADC  with DMA and a timer, I'd put the MCU into other low-power...

lorant124 by Associate III
  • 3559 Views
  • 3 replies
  • 3 kudos

Resolved! STM32F0 FLASH_PROGRAM PAGE BOUNDARY

I'm working on a bootloader with an STM32F072 device. At the end of the programming process, I followed the steps in the link below to switch to the user application:https://community.st.com/s/question/0D53W00000trgpiSAA/how-to-boot-to-random-address...

Custom Bootloader and UART

Hello,I'm using an STM32F205 chip with custom bootloader. I am facing an issue, that when main application is loaded through the bootloader some of the uart's (USART6 and UART4) interrupt transmit (HAL_UART_Transmit_IT()) causes the stm32 to crash. O...

JThom.15 by Associate III
  • 1493 Views
  • 1 replies
  • 0 kudos

Do timers work in CSLEEP or CSTOP modes?

I am going to have an external high speed signal as input to the MCU. I want to use a 32-bit timer to count the number of cycles on that input. Will a regular timer keep counting even in CSLEEP or CSTOP modes? Or do I need to use an LPTIMER. The LPTI...

Resolved! LPTIM2 Pulse Counter

On NUCLEO-H563ZI board I put 3KHz square wave on LPTIM2_ETR (PC4). I want LPTIM2 to continuously count. However the count never increases. LPTIM2 setup...AndClock looks likeMX_LPTIM2_Init() looks likestatic void MX_LPTIM2_Init(void) { /* USER CODE ...

mccabehm_0-1695156427779.png mccabehm_1-1695156480655.png mccabehm_2-1695157445931.png

Resolved! AN3156 and how the MCU bootloader version is reported

Hello,In appnote AN3156 (Rev 14) [USB DFU protocol used in the STM32 bootloader] it saysThe bootloader version is returned in the device descriptor in the MSB of the bcd devicefield (example: 0x2000 = version 2.0).In appnote AN2606 (Rev 59) [STM32 mi...

MButsch by Associate III
  • 4457 Views
  • 3 replies
  • 0 kudos

Rust

Hello, I have a question for you, does the ST company have a program for the Rust language?

AHass.5 by Associate II
  • 3021 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.