STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is HAL_I2C_GetState() required in polling IO mode?

I am using the HAL library with an STM32L07xx processor. To keep things simple, I have implemented master transfers on the I2C bus in the polling IO mode. Most of the time it seems to work, however once in a while a master transmit seems to get lost....

DavePfz by Associate III
  • 2826 Views
  • 1 replies
  • 0 kudos

Resolved! Generated PWM resolution

Hi,I am new to STM32 devices. I have a STM32F407 Discovery 1 board.I wanted to generate a 1 KHZ signal with a 50% duty cycle.The timer clock is configured to 84 MHZI am using TIM3 on channel 4. The prescaler is 210 and the counter period is 400 =>840...

2.png 1.png PXL_20231013_173821654.jpg
BAW by Associate III
  • 2143 Views
  • 1 replies
  • 2 kudos

Resolved! STM32L4 FreeRTOS vs Bare metal performance

Hi, I have an STM32L4x6 processor.I'm reading data using ADC and DMA, and after the HAL_ADC_ConvCpltCallback, I process the data with a Fast Fourier Transform. Originally, in bare-metal, I had a flag in the main loop, and when the interrupt occurred,...

lorant124 by Associate III
  • 2484 Views
  • 1 replies
  • 0 kudos

STM32F4: SD Card as the USB Mass Storage Drive

Posted on December 15, 2014 at 22:02I'm working on a project that has an on-board SD card and a USB port. I'd like to figure out how to connect the SD card to the USB as a mass storage device. Does anyone have any experience doing this and can provi...

rory by Associate
  • 9320 Views
  • 6 replies
  • 0 kudos

TIM1_CH2 breaks down

Hi ST Team,We have an issue concerning a PWM generation.We have a MCU : STM32F303 driving directly the LM25101 driver from Texas instrument with no limiting resistor or other protection on it.The PWM drives two mosfet legs with 2 mosfet configured as...

etour.1 by Associate II
  • 1170 Views
  • 0 replies
  • 0 kudos

STM32 low power standby with 5 wakeup sources?

I would like to build a 5-button remote (RF 868 Mhz) and was thinking of using the STM32G031F6(The RF is provided using an external chip, similar to Si4455)However the STM32G031F6 has only 4 x SYS_WAKEUP pins.Is there anyway to wake up from standby u...

KMill by Senior II
  • 2405 Views
  • 4 replies
  • 0 kudos

Unit Testing in STM32 cube IDE

Hi I need to start unit testing for a STM32 project in C how can I start a the testing, Can any one send some reference for STM32 cube IDE based Unit Testing method

AKHIL6 by Associate II
  • 840 Views
  • 0 replies
  • 0 kudos

Resolved! Port Related Issue

Hello, I was experiencing this weird thing lately with my STM32 Blue Pill board's COM Port.I'm using STM32duino (Blue Pill) with Arduino IDE. I've Already flashed the bootloader and installed the drivers for it. when i connect the board with my PC us...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.