2023-10-11 7:04 PM
Hello,
I'm using an STM32F205 chip with custom bootloader. I am facing an issue, that when main application is loaded through the bootloader some of the uart's (USART6 and UART4) interrupt transmit (HAL_UART_Transmit_IT()) causes the stm32 to crash. Other Uart's are working fine.
If I load the main application without bootloader all the Uarts works without any issue. Are there any ideas about peripherals behavior in application after the jump from a bootloader? Any help would be much appreciated
Thanks
2023-10-12 7:05 AM
Perhaps they are not in a reset state, causing undesired behavior. Debug the code, figure out what "crash" here means in particular and solve it. This is a likely a software bug/issue.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.