STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! BDSL File for STM32H745XIH6

Hello,is somebody is knowing, if a BDSL-File for  STM32H745XIH6  is existing? The affected processor doesn't exist in the "en.stm32h7_bsdl.zip" (https://www.st.com/resource/en/bsdl_model/stm32h7_bsdl.zip) from STM. Five packages are supported, but no...

JPiet.3 by Associate III
  • 1717 Views
  • 1 replies
  • 0 kudos

Resolved! STM32Cube IDE build error

I am working with STM32U575, When building my project I am facing an issue. The error is as follows:C:/ST/STM32CubeIDE_1.13.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin...

Mathil by Associate
  • 2823 Views
  • 2 replies
  • 2 kudos

Resolved! STM32H750 with I2S non blocking-mode (DMA or IT) works only once

Hello,As mentioned in the title, I am trying to output a simple sinusoidal audio over I2S.It works only the first time with DMA and IT, but not afterwards.In blocking mode it works fine. See the code below.Does somebody maybe know why?? (It doesn't m...

pk84 by Senior
  • 6511 Views
  • 10 replies
  • 0 kudos

Resolved! lsm303dlhc.c

Hey st i am working with the stm32f407g and i am trying to make the LSM303 working on my board. At this moment i am using this lib: https://github.com/STMicroelectronics/STM32CubeL4/blob/master/Drivers/BSP/Components/lsm303dlhc/lsm303dlhc.cThe proble...

boot0 config issue without stm32cube programmer

Using STM32 cube programmer I have flashed boot option using option bits and later I have flashed application and It's working fine without grounding boot0 Pin. Is there is any other way to make application start from system memory by configuring opt...

Resolved! need help with STM32H750VB Power regulator voltage scale

hi i have a problem where i want to get the stm to 480Mhz clock but in order to do that i have to set the Power regulator voltage scale to 0 but when i do this the micro controller bugs and i cant connect to it the programmer just say no stm32 found ...

0693W00000Y8LBgQAN.png
bakhti by Associate II
  • 3364 Views
  • 3 replies
  • 0 kudos

TIM DMA not working on STM32F429ZIT

I'm struggling to get DMA working on a PWM Timer. I've read just about everything i can, but  it is not working.Running this code.. produces a PWM signal as expected on the output.  /* USER CODE BEGIN 2 */HAL_TIM_PWM_Start(&htim3, TIM_CHANNEL_2); How...

pwm_3.png SmartSelect_20231011_163256_Gallery.jpg pwm_tim.png TIMp1.png
Heidi by Associate II
  • 4119 Views
  • 6 replies
  • 1 kudos

Semi Hosting to Putty

Hello, MCU:STM32H753XIH6TR Is it possible using an ST Link from a 20 pin JTAG connector to interface with an MCU to send and receive commands via UART to PUTTY/Real Term  perhaps another protocol? I need it to do through the st link to avoid any hard...

LMyle.1 by Associate III
  • 1908 Views
  • 2 replies
  • 0 kudos

Resolved! Minimum setup for STM32H730VBT6 board

Hello.I am very new to ST electronics, though I've spent several years working with chips from another popular manufacturer.I would like to develop a board that prioritizes multiple high-speed gpio lines.I do NOT need:-sdcard, usb, external flash, et...

rbairos by Associate
  • 2037 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.