STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Problems with ST-LINK/V2

Hi,I recently bought a ST-LINK/V2 dongle and it didn't work. I checked the insides of it to see that the microcontroller inside wasn't an ST one, but a Geehy clone microcontroller. I bought another, which was not a dongle, it was the larger white ver...

JS8 by Senior
  • 14035 Views
  • 7 replies
  • 1 kudos

Resolved! Interface with external ADC via SPI at 1MS/s

Hi all,I am using the NUCLEO-F446RE with the STM32F446RE. I am trying to interface with an external dual sampling differential ADC: ADS9224R.ADC Timing DiagramThe ADC can provide samples at up to 3M/s. I would be happy to achieve ~0.8M/s sampling.I h...

0693W00000KZlwCQAT.png 0693W00000KZlxPQAT.png
CPurc.1 by Associate II
  • 18218 Views
  • 27 replies
  • 0 kudos

STM32L083 UART receives only one byte

Hi,I am trying to receive data (on STM32L083) via USART1, the way I was used to doing it on STM32L071. Specifically, I used a circular buffer that was continuously written to by DMA - RX. Now, I've ported the code to this L083 and it seems that nothi...

JR2963 by Senior II
  • 4353 Views
  • 8 replies
  • 2 kudos

STM32 UART Transmit stops responding after some time

Hi all,I am using a STM32L476RG NUCLEO Board with FreeRTOS and STM32 iCUBE LoRaWAN stack. I have a UART interface connected to Raspberry Pi, which periodically sends and receives data to-from STM32. I am using a circular buffer with DMA and IDLE Line...

STM32F103CBT6 Driving PWM for Synchronous DC/DC Buck Converter

Hi,I am quite new to STM32 MCU family and have a quick question. I attached schematic for the reference. Is STM32F103CBT6 capable of driving complementary 50 kHz of PWM signals(HI and LO) with configurable duty cycle for the gate driver IC? Yes, I am...

shin212 by Associate II
  • 3181 Views
  • 1 replies
  • 0 kudos

Maximum analog output voltage from STM32H723ZG

Hi, which is the maximum analog output voltage from the STM32H723ZG? In the datasheet I saw that there are two Op-Amp inside the MCU with gain from 2 to 16. How can I use this Op-Amp? I have to do something about the hardware or I have just to write ...

ECiot.1 by Associate II
  • 3385 Views
  • 5 replies
  • 0 kudos

Resolved! Documentation: USART1/2 and APB2/1 on STM32U5 series

Is USART1 on APB1 (AN5593, tab.17) or APB2 (DS, RM, CubeMX) and USART2 on APB1 (DS, RM, CubeMX) or APB2 (AN5593, tab.17)? Guess, there is an issue in an5593-how-to-use-the-gpdma-for-stm32u5-series-microcontrollers-stmicroelectronics Rv.4 , isn‘t it?

FB1 by Associate II
  • 2139 Views
  • 2 replies
  • 0 kudos

driverchip for GPIO support

Hello forum,I need some hardware help to modify my PCB, which was developed by other people.I use STM32F103. I have one "Master"-Board and several "Slave"-Boards (up to 20) with same controller.Because of current saving reasons I need to set the cont...

APlöt.1 by Associate II
  • 3676 Views
  • 6 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.