2023-10-27 2:57 PM - edited 2023-10-27 2:57 PM
My question is related to the stm32u575 and bu585's board definitions in the Zephyr Project. Actually, there is no question related to the hw design.
I shared these questions on the Zephyr repo but no one has given an answer yet.
https://github.com/zephyrproject-rtos/zephyr/discussions/64276
Regardless of the dev board HW design. I am wondering Why doesn't the 575zi board have board options/configurations/dts design for the tfm build configs and memory partitions while b_u585i_iot02a does. I think this is a common feature of this chip family. So there is a _ns dts board design for b_u585i_iot02a but not for the U575ZI
This is from the b_u585i_iot02a_ns.dts file. I just wanted to calculate total memory size and add all allocated memory regions defined in the dts file and here is the result. ~16kb is missed while the sum of all regions' size is exactly 1mb in the b_u585i_iot02a.dts. Curious why the non-secure config is missing 16kb (normally 2mb = 1024*1024*2 byte = 2,097,152 )
3. Why does the b_u585i_iot02a_ns have a 224kb boot portion size? Is it configurable for the board option _ns
4. Can I use the entire 2mb flash configuration for the u575zi board? Do I really need to have _ns configuration for the u575zi board?
Thank you so much for your help.
Kind regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.