STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST-Link's Mass storage file write from firmware application

Hello everyone,i would like to know if it would be possible to write data on the STLINK mass storage device from the firmware application. This would be really awesome for debugging, logging, testing, etc.I am only aware of dragAndDrop programming fe...

jboui.1 by Associate II
  • 3428 Views
  • 5 replies
  • 0 kudos

Resolved! USART6_CTS pin of STM32F407

Hello forum and devs!Have one simple question: datasheet of STM32F407ZGT (STM32F40x series) and Cube MX says me, that this MCU doesn't contain USART6_CTS pin, but contain two USART6_CK pins. Is it mistake, and where is USART6_CTS pin?Official datashe...

Powerjack_0-1698399674722.png

NiPdAu plating looks like copper finish

We have received   STMICROELECTRONICS SPC58EG80E5QEC0X, the Terminal Plating is Nickel/Palladium/Gold (Ni/Pd/Au), we see that the terminals look copper finish

JKF by Associate
  • 1026 Views
  • 0 replies
  • 0 kudos

Resolved! H743 PLL1 P-divider discrepancy

Hi! I wonder if the P-divider for the PLL1 on the STM32H743 is allowed to be 1.The reference manual (rev. 8 ) states in figure 47 (section 8.5.5) that only values from 2, 4, ... to 128 are allowed. In the register description (section 8.7.13) however...

DanielST_1-1698326008660.png DanielST_2-1698326036426.png
DanielST by Associate II
  • 2374 Views
  • 5 replies
  • 2 kudos

Resolved! Interrupt priority in STM32F429

Good morning, I have some problems with interrupt priority on the STM32F429.I set up a serial communication on UART1 with this priority// USARTNVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn;NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;N...

gerson74 by Associate II
  • 2755 Views
  • 2 replies
  • 1 kudos

Resolved! Unable achieve delay with timer14 in stm32g030kt6 MCU

Hi all,I tried to configure timer 14 to generate interrupt every 500 ms . i am toggling an GPIO to measure delay .when put a breakpoint interrupt gets triggered but unable to see waveform in logic analyser of GPIO toggling with delay .My clock freque...

Nchun.1 by Senior
  • 1870 Views
  • 2 replies
  • 0 kudos

Debugging software in bank2 with dual bank device.

Hello,I'd like to know if there's a way to debug a software running in bank2 of a dual bank flash device, in my case a STM32L476, having the FB_MODE bit set in SYSCTL->MEMRMP register. This would greatly ease tuning the algorithm for flash management...

VBess.1 by Associate III
  • 1212 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.