STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F407VE sampling signal with ADC.

Hello everyone, i'm sampling an analog signal, using an single ADC triggered by a timer, and to observed the reconstructed signal i use a DAC connected to an oscilloscope.I have the next configurations:ADC parameter settings:Clock prescler: PCLK2 div...

yuarth07 by Associate II
  • 3998 Views
  • 5 replies
  • 0 kudos

stm32f429vet6:raw tcp:lwipsetting

kindly suggest lwip setting for stm32cube ide for below for receiving 14000 bytes regularly in tcp raw as clientTcp_Wnd,Tcp_Mss,heap memory size,Pbuf_Pool_BUFSIZEmy values are-:Tcp_Wnd=32000Tcp_Mss,=1436heap memory size,=45000Pbuf_Pool_BUFSIZE=2048i ...

MGOEL.1 by Associate II
  • 1412 Views
  • 1 replies
  • 0 kudos

USB_FS CDC VCP

Hello everyone,I am trying to transfer data to LabVIEW using USB_FS (CDC, VCP). The reason, I shifted to USB_FS (12Mbits/sec) from UART was lower data transfer speed (115200 bps). However, I have one concern regarding USB_FS as CDC. I checked the VCP...

Sheraz2568_0-1698471521058.png Sheraz2568_1-1698471550689.png

STM32H723 FDCAN BOOTLOADER PROBLEM

Hi everyone.I Have worked with STM32h723 arm processor FDCAN bootloader. but I faced a strange problem in writing data into flash. I can successfully make processor go to FDCAN bootloader and get responses from it but can't write data in some address...

majid1 by Associate
  • 11181 Views
  • 7 replies
  • 0 kudos

Resolved! 4 cahannel PWM making (2 ch + complimentory )

Hai ,am trying to make a pwm signal to drive an H bridge driver  ,My board is Nucleo-F070RBI am using the following function HAL_TIM_PWM_Start_IT(&htim1, TIM_CHANNEL_1);HAL_TIMEx_PWMN_Start_IT(&htim1, TIM_CHANNEL_1);HAL_TIM_PWM_Start_IT(&htim1, TIM_C...

Where can I find the STM32 Nucleo Firmware?

I am evaluating the STM32F466RE processor. As part of that effort, I got a NUCLEO-F446RE evaluation board and downloaded the “UM1727: Getting started with STM32 Nucleo board software development tools�? document. Step 3 under the System Requirements ...

AJone by Associate II
  • 5084 Views
  • 2 replies
  • 4 kudos

Resolved! QSPI dual flash - addressing

I'm porting a QSPI bootloader over from a design that 1 flash chip to 2 flash chips in parallel (10 bit mode, common CS).  I am not sure how the addressing works now that there are 2 chips in parallel.  I feel like the only thing STM32 says on the ma...

da66en by Associate II
  • 5938 Views
  • 5 replies
  • 2 kudos

How do I get the frequency of a timer in STM32F769I?

Posted on January 19, 2018 at 13:38I am working with the STM32F7691I-EVAL board and I would like to determine the frequency of any given timer:GET_TIMER_FREQ(TIMx)The macro/function should be able to determine the frequency regardless of which clock...

arnold_w by Senior II
  • 10483 Views
  • 5 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.