STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

IPM30B: minimal working setup

Hello,   Is there any resource or reference available like tutorial video or presentations to set up a minimal working configuration for the IPM30B? I have experience on a low power setup with X-NUCLEO-IHM16M1  but I am new to hardware assemblying wi...

Resolved! Motor Control Workbench MCU selection

Hi,We are working for a project on Railway application, where we have selected STM32G4A1VET6 controller for Motor control application.we are developing custom board for Motor control application, Selected motor is BG65x50 dCore by Dunker motor,above ...

MC_MCU_list_not.png MC_workbench_MCU_list.png
VINODC by Associate II
  • 594 Views
  • 3 replies
  • 2 kudos

Resolved! STSPIN32G4: No errors, but no PWM output

[PN]: STSPIN32G4[VERSION]: v6.4.1[TOOL]: MC Workbench / Motor Pilot[DETAILS]:I am working with a custom PCB design which was largely follows the EVSPIN32G4 schematic. I defined a custom board in MC Workbench and generated firmware, and can upload the...

Motor control connector

Hi ST Team,I'm creating project in the motor control workbench,I had selected hardwars are1. STM32G4EVAL1 Board2. Motor Drive3. Motor once i selected in the tool as shown in below.in this connector are not available to connect to the main board to mo...

Motor_Connector.png
VINODC by Associate II
  • 363 Views
  • 3 replies
  • 0 kudos

Six-Step Bug

Hello, i found a bug in the code generated by the Motor Control Workbench usign the 6-step algorithm. Even with Open Loop mode enabled, the code is still using the PID for the initial duty cycle computation (state CHARGE_BOOT_CAP in the TSK_MediumFre...

Leo4 by Associate II
  • 282 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.