STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9744 Views
  • 5 replies
  • 3 kudos

Sensor switch in motor control with FOC algorithm

I am using the EVLSPIN32G0B1 demo board and the MC Workbench v6.4.1 software, and I would like to use the FOC control algorithm.More specifically, I would like to use the Hall sensors when the motor starts and operates at low speeds, and then switch ...

Diego3 by Associate
  • 521 Views
  • 3 replies
  • 0 kudos

Vertical Take off in STEVAL FCU001

Hi All,I am beginner to drones. We assembled one drone using STEVAL FCU. 002. board ,  recommended set. of motors and. propellers along with battery. We Chose different. frame.  than. one recommended . It is smaller in size. While flying , vertical t...

mmdave1 by Associate III
  • 12024 Views
  • 30 replies
  • 5 kudos

Motor will stop after ramp p

[PN]: custom Board based on evspin32g4-dual[VERSION]: 6.4.0[Motor]: Xing2207 1800Kv[CubeMx]:6.14.1Hello,I have a problem with getting my FOC BLDC motor to start, the specs of the motor are: 0,08Ohm 50uH 0,32Vrms/kRPM. My project is for two sensorless...

Screenshot 2026-03-17 181420.png Screenshot 2026-03-17 180627.png Screenshot 2026-03-17 181250.png
QuirinS by Associate III
  • 270 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.