2026-04-09 5:08 AM - last edited on 2026-04-09 5:30 AM by Peter BENSCH
2026-04-09 5:47 AM
Welcome @gabriele_deboni, to the community!
The STEVAL-IPM30B is an IGBT-based SLLIMM (Small Low-Loss Intelligent Molded Module) power stage STGIB30M60TS-L, so it is mainly intended for higher motor voltages. Due to the relatively high IGBT saturation voltage of IGBT, it is not a good fit for a 24V PMSM minimal setup. The STEVAL-IPM30B is specified for a minimum DC bus voltage of 125V.
For your use case, a low-voltage, MOSFET based reference design would be more appropriate, e.g. the EVSPIN32F0251S1 or the EVALSTDRIVE101?
Regards
/Peter
2026-04-09 6:23 AM
2026-04-09 6:37 AM
You can find all available documentation on the product website of the STEVAL-IPM30B, whose function is described in detail in UM2709. Further startup assistance can be provided by the power FAE of your local distributor.
Good luck!
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.