STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1837 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4991 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9744 Views
  • 5 replies
  • 3 kudos

STSPIN32G4: No spin with encoder as main sensor

[PN]: STSPIN32G4 (custom board), AMT103 encoder[VERSION]: MCSDK v6.4.1[TOOL]: MC WB[DETAILS]:I need to implement torque control for my custom board and BLDC motor using a quadrature encoder as the primary feedback sensor.First, I successfully profile...

ClyneModa by Associate II
  • 830 Views
  • 10 replies
  • 0 kudos

Resolved! STEVAL-CTM009V1 for ACIM FOC Control

Hi everyone,I’d like to learn more about FOC algorithms and eventually design my own motor driver. For this purpose, I’m planning to use the STEVAL-CTM009V1 to drive a pump or traction motor similar to those used in forklifts.In general, forklifts wi...

Ymtr by Associate
  • 406 Views
  • 3 replies
  • 0 kudos

Rotor starts in wrong direction sometimes.

I'm using an STM32G431 and MCSDK 6.4.1. It's a 340 VDC BLDC motor with two pairs of magnets, running in FOC mode with HAL sensors. The motor works well most of the time, but it often starts in the wrong direction and then returns to the correct direc...

BlachaL by Associate
  • 187 Views
  • 1 replies
  • 0 kudos

BLDC: Delete the Alignment phase of the encoder

Hi all,I noticed that when using the encoder, the motor undergoes an alignment phase during which it completes a rotation until it reaches the position where the Index Z signal is triggered.I was wondering if it's possible to skip this alignment phas...

JulesC by Associate III
  • 388 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.