STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Regarding issue : STEVAL-SPIN3202 design

I have used STEVAL-SPIN3202 evaluation board for Pump application after finalizing the code i have tried to make my custom board from the existing schematic but faced with many issues as listed below1) From the existing schematic i have removed the p...

Shubham08 by Associate III
  • 3597 Views
  • 7 replies
  • 1 kudos

EVSPIN958-SingleMotor firmware

Hi, i'm using NUCLEO-F401RE product with EVSPIN958 expantion board connected to, for motor control.I've connected this with STSPIN Studio 2.0, it's running correctly with EVSPIN958-SingleMotor firmware (i'm using DC brushed motor).i'm just searching ...

de82 by Associate
  • 1313 Views
  • 1 replies
  • 0 kudos

X-Nucleo IHM07M1 Voltage

Hi,I am learning motor control by using ST Motorcontrol workbench. I'm using P-NUCLEO-IHM002 pack which contains NUCLEO-F302R8, X-NUCLEO-IHM07M1 and power supply.While I trying to use this board, in the user manual they said some changes in the jumpe...

Sanjay_Periyasamy_0-1741414179590.png

Guidance regarding motor controller

Hey,I have started working on electronic speed controller, want to build esc with trapezoidal and FOC algorithm with sensorless schemes for unmanned aerial vehicle(drones)Can anyone suggest the solution available on st for the same.it will be great h...

Anmol by Associate
  • 955 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.