STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

Resolved! Cant see the pwm from nucleo h755ziq

i generated the code using the workbench for stm32h755ziq and the motor driver ihm07m1 with a 12v bldc motor...and i have called the api's for motor start as well in the main code ...but after downloading it into nucleo..i cant see any pwm signals on...

2 Motors with STM32H755ZI

Hi, I managed to create a custom inverter board using STMC Board Designer which is basically 1 Nucleo-H755ZI-Q inverter and 2 times a IHM08M1 power board(see Other post about creating bridge ) . One of the 2 power boards is therefore connected to oth...

Zeno by Associate III
  • 2864 Views
  • 5 replies
  • 0 kudos

Resolved! Setting motor parameters: Rs, Ld and Ld/Lq ratio

I have 5kW QS138 BLDC motor within my e-bike project with my own motor controller electronics. I have measured inductance and series resistance from the motor with a precision LCR meter: Lq [mH]Rs [ohm]Ld [mH]Rs [ohm] Ld/Lq       120 Hz0.0310.0030.02...

Hall Phase Delay

Hello,I need confirmation that the Hall Delay in the below waveform i have taken is 180Degrees. Hall sensors are 120Degrees apart as below in the diagramI find the motor running in reverse direction. 

STUser34_0-1742287205049.png
STUser34 by Associate III
  • 1288 Views
  • 2 replies
  • 1 kudos

Resolved! Current sensing circuitry

Hi, I am working on developing a new motor driver using ST motor control.I am trying to understand current sensing circuitry (three shunt resistors) but I don't understand the offset circuitry as shown in this picture: As I currently understand it th...

Jelmer_0-1742564764155.png
Jelmer by Associate
  • 2607 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.