cancel
Showing results for 
Search instead for 
Did you mean: 

FOC, Position Control used but MCM_POSITION_CONTROL of MC_ControLMode_t never used

Zeno
Associate III

Hi, 

[PN]: Nucleo-H755ZI-Q; IHM08M1
[VERSION]: MCSDK 6.3.2
[TOOL]: Firmware programming - Position Control mode
[DETAILS]: MC_ControlMode_t never set to MCM_POSITION_MODE. When a position command is executed the LastModalitySetByUser is set to MCM_TORQUE_MODE. The MCM_POSITION_MODE is never used, nowhere in the code is there any trace of that state.
[EXPECTED BEHAVIOR]: When executing 
MC_ProgramPositionCommandMotor1() I expected the LastModalitySetByUser to be set to MCM_POSITION_MODE.


[HOW TO REPRODUCE]:configure MC Workbench project with 1 motor and enable position control, check the code generated in mc_interface.c following the function api function MC_ProgramPositionCommandMotor1():

/**
  * @brief  Programs a motor position ramp
  *
  * @PAram  pHandle Pointer on the component instance to work on.
  * @PAram  FinalPosition The desired rotor position in radians.
  * @PAram  Duration The duration of the movement to reach the final position, in seconds.
  *
  *  This command is executed immediately if the target motor's state machine is in
  * the #RUN state. Otherwise, it is buffered and its execution is delayed until This
  * state is reached.
  *
  * Users can check the status of the command by calling the MCI_IsCommandAcknowledged()
  * function.
  */
__weak void MCI_ExecPositionCommand(MCI_Handle_t *pHandle, float_t FinalPosition, float_t Duration)
{
#ifdef NULL_PTR_CHECK_MC_INT
  if (MC_NULL == pHandle)
  {
    /* Nothing to do */
  }
  else
  {
#endif
    pHandle->pFOCVars->bDriveInput = INTERNAL;
    float_t currentPositionRad = (float_t)(SPD_GetMecAngle(STC_GetSpeedSensor(pHandle->pSTC))) / RADTOS16;
    if (Duration > 0)
    {
      TC_MoveCommand(pHandle->pPosCtrl, currentPositionRad, FinalPosition - currentPositionRad, Duration);
    }
    else
    {
      TC_FollowCommand(pHandle->pPosCtrl, FinalPosition);
    }

    pHandle->LastModalitySetByUser = MCM_TORQUE_MODE;
#ifdef NULL_PTR_CHECK_MC_INT
  }
#endif
}
pHandle->LastModalitySetByUser = MCM_TORQUE_MODE;

 

I assume that this is bug and that this needs to be MCM_POSITION_MODE. I've checked the .ftl files as well and the origin of the bug is in the mc_interface.c.ftl file: 

<#if MC.M1_POSITION_CTRL_ENABLING == true || MC.M2_POSITION_CTRL_ENABLING == true>
/**
  * @brief  Programs a motor position ramp 
  *
  * @PAram  pHandle Pointer on the component instance to work on.
  * @PAram  FinalPosition The desired rotor position in radians.
  * @PAram  Duration The duration of the movement to reach the final position, in seconds.
  *
  *  This command is executed immediately if the target motor's state machine is in 
  * the #RUN state. Otherwise, it is buffered and its execution is delayed until This
  * state is reached.
  *
  * Users can check the status of the command by calling the MCI_IsCommandAcknowledged() 
  * function.
  */
__weak void MCI_ExecPositionCommand(MCI_Handle_t *pHandle, float_t FinalPosition, float_t Duration)
{
#ifdef NULL_PTR_CHECK_MC_INT
  if (MC_NULL == pHandle)
  {
    /* Nothing to do */
  }
  else
  {
#endif
    pHandle->pFOCVars->bDriveInput = INTERNAL;
    float_t currentPositionRad = (float_t)(SPD_GetMecAngle(STC_GetSpeedSensor(pHandle->pSTC))) / RADTOS16;
    if (Duration > 0)
    {
      TC_MoveCommand(pHandle->pPosCtrl, currentPositionRad, FinalPosition - currentPositionRad, Duration);
    }
    else
    {
      TC_FollowCommand(pHandle->pPosCtrl, FinalPosition);
    }
  
    pHandle->LastModalitySetByUser = MCM_TORQUE_MODE;
#ifdef NULL_PTR_CHECK_MC_INT
  }
#endif
}
</#if><#-- MC.M1_POSITION_CTRL_ENABLING == true || MC.M2_POSITION_CTRL_ENABLING == true -->
</#if><#-- FOC -->

 

2 REPLIES 2
GMA
ST Employee

Hello @Zeno,

You are right, MCM_POSITION_MODE is defined but not used.
On the other hand, as mentioned on AN5464 Position Control application note: "Current control for field orientation (FOC)".
It means that TORQUE mode is used for position control feature (refer to "2. Algorithm description").

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA
Zeno
Associate III

Hi @GMA , 

Thank you for the quick response. 

Yea I figured that Postion Control mode is basically constantly adjusting "jerk", i.e. Torque.

But still the overlying control modality needs to be position control since it's description says:

MCM_POSITION_MODE, /**< @brief Closed loop, sensored position control mode. */
 
If it comes to swapping between control modes this state should be correctly reflected if a Position Control command was/is executed no?
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.