STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

DC MOTOR DRIVER

We are currently using a DCX32L motor rated at 12V and 160W, and ourmain objective is to achieve constant torque. Specifically,we need a solution that integrates current sensing with an interface that permits real-time control via software. Is this p...

spolaka by Associate
  • 883 Views
  • 1 replies
  • 0 kudos

Control 3 phase motor with STEVAL-IPM15b

Hello,​I am trying to drive a three-phase motor with the STEVAL-IPM15b, but it is not working properly. I applied 15V to Vcc and 125V or 150V to Vdc and tried testing, but the motor did not run. I checked TP5, TP12, TP6, and TP7 with an oscilloscope,...

gateSignal.png
221 by Associate
  • 979 Views
  • 1 replies
  • 0 kudos

Noisy Torque/Phase Currents

I have a custom board, which is based on the STEVAL-SPIN3201, it is used to control a low inductance BLDC motor with hall-sensors (100µH). The motor controller is running and is able to control the motor. Unfortunately the phase currents tell that th...

Nikolaj_TL_2-1732889507293.png

Resolved! TRIG_X Signal with the STEVAL-PTOOL4A

Hello,I am reading the documentation of the STEVAL-PTOOL4A, I have noticed that it is equipped with a TRIG_X  to enable/disable the DC/DC booster. I don't know if I understood well its functionality, but It will mainly turn on/off all the board inclu...

AnthonyK by Associate III
  • 1278 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.