STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! HAL_NVIC_SystemReset() don't work on STM32H755

hello ST Community, I'm developing the bootloader for the STM32H755 microcontroller from a specific flash memory address of 0x08010000. I also modified the USER_VECT_TAB_ADDRESS definition in the file 'system_stm32h7xx_dualcore_boot_cm4_cm7.c', as fo...

image.png
Domy_ST by Senior
  • 257 Views
  • 1 replies
  • 0 kudos

Resolved! Impact of changing ThreadX timebase to 1ms

I have changed the ThreadX system timebase on an STM32H7 from 10 ms to 1 ms (i.e., the RTOS tick is now 1 ms). The application is quite large and makes extensive use of ThreadX services such as thread delays, semaphores, mutexes, event flags, and tim...

Configuring External XSPI PSRAM on STM32H7R

Hi all, I am trying to bring up a new custom board with an STM32H7R7 and external flash as well as external PSRAM. While I managed to get the external flash working after some try and error, the external PSRAM seems to be more stubborn. The board use...

SaschaK by Associate II
  • 780 Views
  • 7 replies
  • 7 kudos

Resolved! stm32n6 PPS in (ETH_PTP_AUX_TS)

Hello,I need to sync the stm32n6 system timer to be used as PTP master. According to the Reference Manual there is a PPS input that can generate timestamp and interrupt: ETH_PTP_AUX_TSBut according to the RM it is not in all models, and I can't find ...

Noam_h by Associate II
  • 999 Views
  • 11 replies
  • 0 kudos

STM2WBA65RI Low-Power Mode (STOP2)

Hello, I am currently using the STM32WBA65RI development kit and exploring its low-power modes. I have run the STOP2 mode example and, according to the datasheet, the current consumption in this mode should be around 5 µA. However, I am measuring the...

JPortilha by Associate III
  • 463 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.