STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC DMA Multiple channel

Post edited by ST community moderator. In next time please use </> to share a code. HI, I have Implemented ADC1 - DMA with one channel and ADC2 - DMA with 7 channels and im transmitting data through UART IT. I want to know if this code works usually....

Resolved! OpenAMP RPMsg data loss from M4 to M7 core

Hi,I am using STM32H755 where M7 and M4 runs bare-metal firmware using OpenAMP (RPMsg).Sampling rate is set to 250 SPS. The data is sent from M4 to M7 using OPENAMP_send() function.Observation: Data loss of approximately 10% is observed during transm...

MX66LM1G45G_STM32U5G9J-DK2.stldr

I am developing a project using the STM32U5G9J. In particular I based our board on the STM32U5G9J-DK2 board. My project includes over the air update for which I am using the external flash that comes on the DK2 board for temporary firmware swapping s...

Resolved! LwIP: can't find fs.c; needed by fs.o

Hi,I am new to ST platform, i am facing an issue as below.C:/Users/Yuvaraj/Desktop/Test/1/Middlewares/Third_Party/LwIP/src/apps/http/fs.c', needed by 'Middlewares/LwIP/apps/http/fs.o'. StopI am opened the project from examples codes.Can anyone help ?...

Yuvi89 by Associate II
  • 509 Views
  • 6 replies
  • 2 kudos

USB PD (UCPD) on STM32H562

Hi,I´ve problems getting UCPD running on a STM32H563. With STM32G0 I´ve alraedy realized a lot of such projects with UCPD. Hence I suggest, that it maybe is a problem of the DMA which is much more complicated to configure on the H5. Is there any info...

AWack by Senior
  • 1940 Views
  • 12 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.