STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

IEC 60730 Class B compliance for STM32G031xx

Hi Support Team,   I am currently using the STM self-test library to ensure compliance with IEC 60730 Class B requirements. Specifically, I worked with the example package X-CUBE-CLASSB-G0 v4.0.0 on the NUCLEO-G071RB platform, utilizing the provided ...

Aayush by Associate
  • 373 Views
  • 3 replies
  • 0 kudos

Resolved! STM32U5A9 and X-CUBE-AUDIO?

Hi,I'm getting info on playing mp3 files with my custom Nucleo-U5A9 (originally a NUcleo-U575, I replaced the MCU and added xtal). I'll be using the audio codec TLV320AIC3110 with I2C and SAI from the U5A9. I'll be using ThreadX, FileX an a uSD card....

Rodo by Senior
  • 707 Views
  • 4 replies
  • 1 kudos

STM32H735G-DK can't change pixel format mode

Hello,I'm working on the STM32H735G-DK and try to change LTDC pixel format mode on the fly, but it doesn't work. I'm using the BSP example from example board pack in CubeMX for this board. After reset is possible setup the first time pixel format, bu...

wegi01 by Associate III
  • 320 Views
  • 2 replies
  • 0 kudos

Resolved! Use external NOR flash to move CPP object file

Hello,I have STM32F7 controller, using Free RTOS, trying to interface external NOR flash, S29GL128S10TFIV13.I have one source file say testCode.cpp, which I want to move completely in external NOR flash, but every time I ran then code it give Hardfau...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.