STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! g431kb low output voltage

Hello,Newbie here got nucleo-g431kb and I was trying to power a sensor from either CN3 pin 4 at 5V or CN3 pin 14 at 3.3V, but neither pin outputs the correct voltage. Pin 14 outputs ~300mV and pin 4 outputs ~450mV. This is also with no external load,...

dfiallo by Associate
  • 1224 Views
  • 2 replies
  • 2 kudos

Resolved! How to change VSO0 to VSO1 in RCC?

I am using nucleo-g491re and i was unable to use prescale of 1 asynchronous for my ADC. the solution, on this site, was to change VSO0 to VSO1 but it seems my board has no such option. only to boost (whatever that means). So how can i get the maximum...

AdilMC_0-1739079037013.png
AdilMC by Associate II
  • 1499 Views
  • 2 replies
  • 0 kudos

Resolved! Nucleo-H7A3 Error: No STM32 target found!

I'm trying to get a nucleo-H7A4 getting to run my code.Only I got this message now:     -------------------------------------------------------------------                      STM32CubeProgrammer v2.4.0                      -------------------------...

Evan .1 by Associate II
  • 3580 Views
  • 6 replies
  • 1 kudos

Resolved! STM32F103C8T6 USB sanity check

Hi All, sanity check sought:I'm using the blue pill (STM32F103C8T6) for a audio project powered & controlled through the serial/USB.I'm using the STM32 cube and a dev board for the s/w which looks ok; in terms of software I've followed https://contro...

JFren.1 by Associate
  • 1494 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.