Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hi everyone. Im using the nucleo-h743zi2 and im facing the following issue: When trying to printf using redirect to usart3 with the following clock settings: /** * @brief System Clock Configuration * The system Clock is configured as fol...
In STM32H757XIH6, is SMPS GND and VSS internally shorted inside the IC or should be shorted externally during layout stage. Snips supporting these are attached.
Hello ST and community members,I am writing to ask for help with a persistent issue regarding the Virtual COM Port (VCP) feature on the STLINK-V3MINIE.SummaryI have two STLINK-V3MINIE units, and on both of them, serial communication via the VCP does ...
good morning, I am wondering what the DNF means in my datasheet: does it mean there is no connection between pb3 and the LED? then i am wondering if i can use PB3 for other instances, and i am also wondering why there is this DNF instead of just not ...
I am trying to get shutdown and wakeup working using the blue top switch on the Nucleo-L433RC-P board.I have set GPIO pin PC13 to SYS_WKUP2...Below is my code...HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN2); while (1) { status = HAL_GPIO_ReadPin(GPIOC, P...
I am a beginner at stm32 Nucleo board, when I connect the board and the Lap, LD5 turns green but LD4 turns to green/red blinking, which means the voltage is correct but the MCU has no response or connection error. Could you please help with that?
I'm working with the NUCLEO -F 446ZE MB1137 B-01 development board. My goal is to make a Virtual Com Port tunnel, where I plug in PA11/PA12 (USB device) to a PC and PB14/PB15 (USB host) to another product my company makes. I want to use the full spee...
Hello, I have been having issues trying to get my STM32F411 PCB working with the USB-C bootloader, currently the device is not even being recognized at all by my computer. When checking with a multimeter I have found that D+ is not pulled high by the...
Dear all,I try to use ST-LINK USB Type-C to debog in CubeIDE IDE, however I have such error on CubeProgrammer by connecting the ST-link (see Picture 1). In CubeIDE, i have a different error (see Picture 2). The Nucleo is configured according to the d...
Iam Using 2 STM32F407VGT6 board one as master and another board as slave from Master side it is Transmitting but slave is showing the Bus error both Master and slave iam using in the inturrept mode
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.