Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hi ST Community,I have developed a custom board based on the MB997E evaluation board as a reference design.1. Could you please help me review my custom board design and schematic to identify any possible mistakes.2. In my custom design, I have also a...
I am using the Nucleo-L433RC-P board but having difficulty flashing and debugging. 9 out of 10 times I get the following error...STMicroelectronics ST-LINK GDB server. Version 7.11.0 Copyright (c) 2025, STMicroelectronics. All rights reserved. Star...
It seems that the STLINK-V3SET is out of stock almost everywhere. Is there any information on when it will be back in stock?Thanks
Hello everyone,I've noticed that several users have experienced issues related to the LDO power supply setup for the STM32H757A. I’m currently working on a design using this MCU in LDO mode, and I’d like to confirm whether my power supply implementat...
I want to let the user LEDs blinken, however it is not working. When I run the code the LD4(COM) is blinking red and green. after the run the LD4(COM) is red the whole time and the user LEDs do not blink. Should the LD4(COM) be lighting green?
Hi Community,I am about to work on STM32H7471-DISCO Development BoardCan you provide Schematic of this Board.I found all the technical documents from https://www.st.com/en/evaluation-tools/stm32h747i-disco.html# but I do not found board schematic.
Hi, I am using Nucleo-144 boards in my project where I have changed the clock source for STLINK IC to external crystal using STLINK firmware upgrade tool. Before it was HSI/2 =8MHz. Now I am trying to revert the configuration back to 8MHz but I am no...
I am using the Nucleo-L433RC-P board and want to use LPUART RX on pin PA3.But the schematic shows that pin PA3 is used for STLINK_RX. What is STLINK_RX / STLINK_TX used for ?Can I remove SB75 to access the pin or would this stop STLINK from working ...
stlink-V3pwr current : 21mA X-NUCLEO-LPMO01A current :17mA actual current : 15mA
Title edited to "STLINK-V3MODS"Hello ST,Do you perhaps have an STEP or IGS file of the STMV3MODS module ?Thank a lot.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.