2025-07-15 5:21 AM - edited 2025-07-15 5:21 AM
Dear all,
I try to use ST-LINK USB Type-C to debog in CubeIDE IDE, however I have such error on CubeProgrammer by connecting the ST-link (see Picture 1). In CubeIDE, i have a different error (see Picture 2). The Nucleo is configured according to the default configuration in the documentation (jumper on BOOT0, BOOT1 & 1-2 to CN9)
Sincerely,
Solved! Go to Solution.
2025-07-15 5:41 AM - edited 2025-07-15 5:45 AM
Hello @qmarecat and welcome to the Community,
Could you specify the version of STM32CubeProgrammer ?
I recommend you follow these guides for debugging:
You can also refer to the videos about advanced debugging with CubeIDE: STM32CubeIDE Advanced Debug Features.
2025-07-15 5:41 AM - edited 2025-07-15 5:45 AM
Hello @qmarecat and welcome to the Community,
Could you specify the version of STM32CubeProgrammer ?
I recommend you follow these guides for debugging:
You can also refer to the videos about advanced debugging with CubeIDE: STM32CubeIDE Advanced Debug Features.
2025-07-15 6:04 AM
Dear Imen,
thank you for your Answer,
I found how to do by switching up the BOOT1 jumper to 1 instead of 0.
Sincerely
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.