Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
I'm working on a project requiring me to save a frame captured by a camera to an SD Card. I'm using SPI to do this. I am able to save the image from an OV5640 camera to sram in a buffer using DMA, where the size is more than 300,000 bytes. I am able ...
What is the lens used on the B-CAMS-OMV kit? Or, what is the field of view? or, what is the focal length?
I have this SRC1m1 board and would like to run some tests with it at 20V. Your user manual is conspicuously not mentioning running it above 5V. It does have a lot to say about running it at 5V if you do not have UCPD. Sortof implying if you do have U...
Hi everyone, I am currently having the problem, that I cannot flash a working Program to a new STM32f746G-DISCO.The Software Is already written, and runs on 6 other STM32f746G_DISCO Boards, that were ordered in 2021.Now I wanted to flash this exact S...
Original title: Facing a debug issue. the code works in another board and gets firmware update. but its not working in my current stm32f103zet6 customized board.Shortened in accordance with Posting Guidelines .
I am trying to work on STM32F439ZIT6 using its respective Nucleo board. I am not able to generate an ioc file even after installing the latest version 1.28.2 in STM32F4 series. Why is this happening and how can i resolve this issue?RegardsavbST
My STlink V2 is not being detected. I bought an original stlink but it's still not being detected. I had a clone previously. It's frustrating why it's only happening with me. It says could not verify ST device. When I update it it says can't detect S...
Hello everyone,I've designed a development board featuring an on-board STLink (based on STM32F103CBU6) and an on-board MCU (STM32H753VIH6. However, I'm encountering a frustrating issue with the on-board STLink functionality.I've flashed the STLinkV...
Hi,I am using the ST link V2 debugger and i have updated the firmware using stm32 programmer software and used the stsw-link009 and when i tried connecting it shows me some below errors. After updating the firmware it worked for few moments and then...
Hi,I have STM32H757I-EVAL board which has MB1166 Rev A LCD daughter board. I tried to find which display controller is used with this LCD display. I had gone through the MB1166 schematics which shows 2 options 1. KM-040TMP-02 2. FRD397B2509I got con...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.