2025-07-15 11:52 PM - last edited on 2025-07-16 12:48 AM by Andrew Neil
good morning, I am wondering what the DNF means in my datasheet:
does it mean there is no connection between pb3 and the LED? then i am wondering if i can use PB3 for other instances, and i am also wondering why there is this DNF instead of just not connecting PB3 and the LED
Best regards
Solved! Go to Solution.
2025-07-16 12:34 AM
> can i still use PB3 as GPIO input from the nucleo header for another use?
In theory yes.
UM2397 states:
LD2 USER
This green LED is connected to the following STM32G4 I/O:
• PB8, if the configuration is SB7 ON, and SB6 OFF (default configuration)
• PB3, if the configuration is SB7 OFF, and SB6 ON
But according to the schematic PB3 is also connected to T_SWO via SB4, so it is connected to the onboard ST-Link.
So if you want to use PB3 as GPIO it will be necessary to open SB4, and you will lose SWO.
2025-07-15 11:59 PM - edited 2025-07-16 12:01 AM
DNF = "do not fit"
Keep it open usually (or think about before closing)...
And yes, you can use PB3 for any other purpose, since it is not connected to LD2.
2025-07-16 12:02 AM
so it means that the solder bridge do not fit?
can i still use PB3 as GPIO input from the nucleo header for another use?
thank you for the quick awnser
2025-07-16 12:34 AM
> can i still use PB3 as GPIO input from the nucleo header for another use?
In theory yes.
UM2397 states:
LD2 USER
This green LED is connected to the following STM32G4 I/O:
• PB8, if the configuration is SB7 ON, and SB6 OFF (default configuration)
• PB3, if the configuration is SB7 OFF, and SB6 ON
But according to the schematic PB3 is also connected to T_SWO via SB4, so it is connected to the onboard ST-Link.
So if you want to use PB3 as GPIO it will be necessary to open SB4, and you will lose SWO.
2025-07-16 12:53 AM
@Jad wrote:so it means that the solder bridge do not fit?
Exactly.
It means that it is not fitted during manufacturing - but left there as an option for the user fit, if required.
It is pretty common throughout the industry - not specific to ST or STM32
Sometimes you will see similar terms like DNP = Do Not Place, etc ...
eg, https://fedevel.com/forum/beginners/423-dnf-do-not-fit-components
#DNP #DNF #NotFitted
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.