2026-03-14 4:24 AM
Hi ,
Recently I got a NUCLEO-C051C8 board and tried to connect it to windows and program it using STm32CubeIDE but it does not show that st-link is connected , ST-link on board blinks RED continuously.
Cant install it ( installation goes through , but cant see it in device manager ) using stsw-link009
( https://www.st.com/en/development-tools/stsw-link009.html?dl=redirect )
Cant connect using STM32CubeProgrammer.
Tried 2 USb cables , various ports of pc but in vain.
Can someone please help ?
Solved! Go to Solution.
2026-03-17 10:51 PM
Thanks , I am able to make it work now.
Seems like I had to remove Jumpers from CN-2 and it did usb enumaration ( Red LED went steady ).
Thanks a lot for your help.
thanks & warm regards,
~ Rudresh
2026-03-14 6:34 AM
Blinking red LED means it's not enumerating. Usually due to using a power-only USB cable. Try a different USB cable or a different USB port.
Even if drivers aren't installed, something should show up in device manager as an unknown device.
2026-03-16 3:42 AM - edited 2026-03-16 3:43 AM
Hello @rudreshjoshi and welcome to the community;
Could you please take a look at this article How to solve connection errors when connecting and programming the STM32 target board may help you to solve the issue.
Thank you
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-03-16 3:59 AM
As @TDK said, try a different cable - make sure it's one that actually gives a data connection with other devices.
More things to try here.
2026-03-17 10:51 PM
Thanks , I am able to make it work now.
Seems like I had to remove Jumpers from CN-2 and it did usb enumaration ( Red LED went steady ).
Thanks a lot for your help.
thanks & warm regards,
~ Rudresh
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.