2026-03-17 2:47 AM - last edited on 2026-03-26 3:51 AM by KDJEM.1
Hi
2026-03-17 8:42 PM
Question:
Does measuring current at this point (CN2 pins 3 & 4) isolate the consumption of the NPU and CPU (VDDCore)? Specifically, I want to know if this measurement will include the power draw from the camera module and LCD display if they are active in the same project.
brief answer (answer from glance, not fully correct):
measuring current at this point (CN2 pins 3 & 4) will not isolate the consumption of the NPU and CPU (VDDCore).
this measurement will not include the power draw from the camera module and LCD display if they are active in the same project.
2026-03-17 10:32 PM
HI @jiangfan
I am planning to compile the Model(STM32 Cube AI studio) with and without Neural-ART. Then planning to measure current follow from CN2-3 to CN2-4 separately for the two models compiled(with and without Neural-ART). Hope this will give current consumption during CPU operation and Current consumption during CPU + NPU operation.
1) Is it possible to use the same pin for measuring current consumption in both CPU-only and combined CPU + NPU processing modes?
2) Could you please confirm that does the pin i have selector is correct or not for the current measurement(I am powering the board via CN6)?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.