Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hi, Apologies in advance for my ignorance. I have a NUCLEO-G491RE and want to use it as a USB CDC. Unfortunately I haven't had any success getting it to work. My problem is that doesn't even appear to show as a device on the host. I have looked at s...
What is the proper way to power the STM32 Discovery Kit externally without USB.
Hi! I am new in electronics, but I am trying to design my PCB using STM32F469IIT6. I did a similar project before using a simple atmega168, but the STM32 seems way more complex. I wonder what the minimum of hardware connection is I need to be able to...
Hello STM32 Folks,I was hoping to get some information regarding VBAT on STM32U5 MCU. I am currently powering the STM32U5 MCU with 1.8V (VDD supply). I need to have external clock oscillator for the Real Time Clock that is powered by VBAT (Coin Cell ...
Hello STM32 community,I'm encountering an issue with my STM32L562VET controller where the debugger gets stuck at the `HAL_GetTick()` function. When debugging, the program seems to halt at this point, making it difficult to proceed with the debugging ...
please suggest delevopment board for STM32L462CEU6.
Hi,I tried to explore the STM32CubeExpansion_CELLULAR package to change the code according to my need. In that process I am lost. Can anyone guide me on which file should I focus on changing the code? This is too much of code to start with. I have al...
Hello, I would like to build a exension board for my ST-LINK V3 to have a custom connector output. To save time and avoid positioning error, where could i get gerber of one of the extension board (MB1440C or MB1599B) ? i just need board edge cut and ...
How does one connect the STLink debug port to an older target with 0.025 square posts on 2.54 mm ptch for the debug connections? As best I can tell, the supplied cables only support 1.27 mm pitch,
Is the a User Manual available for the Nucleo-N657X0-Q that contains the connector pinouts and jumper settings etc. The document (UM1727) listed on the documentation page https://www.st.com/en/evaluation-tools/nucleo-n657x0-q.html#documentation point...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.