STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Debugging NUCLEO-H723ZG

Does any one know if this board can be debugged via the USB port that is connected to the PC or does one require an external debugging link?If external is required which one would you guys recommend I do have ST-LINK V2 which I use for smaller boards...

erastusC by Associate III
  • 3204 Views
  • 7 replies
  • 2 kudos

ST-LINK V3 is not working

Hello, I have two STLINK-V3 programming devices. But I can't program or debug. When I try to connect to my device with STM32CubeProgrammer, I get the errors "Unable to get core ID" and "No STM32 target found! If your product embeds Debug Authenticati...

MTURAN by Associate
  • 3589 Views
  • 5 replies
  • 2 kudos

Low consumption NucleoL476RG

Hello community, I have been working with the nucleol476rg in low power modes, but I have had some doubts during the tests I have performed, specifically using the stand by mode, I understand that only the RTC is active in fact with it I set the alar...

CamiloRJ9 by Associate II
  • 1580 Views
  • 3 replies
  • 2 kudos

ADC DMA stm32f401

Can the ADC write to the buffer faster than the buffer values are sent to PC?- Single channel ADC using DMA, non-circular, EOC every conversion- ADC is in 12-bit resolution but as I understand it writes a full 16-bits each conversion - Buffer size 10...

Using USART1 Rx on STM32H750B-DK

Hi , I am trying to use the USART1 to talk to another device which is runnig UART and sending and receiving data. I am able to see that the data from USART1 Tx (STM32) is received on the other device but the data being sent from the other device is n...

nsingh by Associate II
  • 3252 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.