Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello,I'm interested in Power Line Communication and the X-NUCLEO-PLM01A1.I would like to confirm before purchasing. What is the role of the PLM connector (CN1)?Is it a PLC line? If so, is the Lab DC Supply Inout Connector (CN2) just a power supply?...
Hello i m would to learn how to debug the h743, h753, f407, and f410 nucleo board using the STLINK-V3 module, i know the H743 Nucleo board has a build-in stlink, but i just wanna learn to use this STLINK-V3 before my custom design board is ready. Can...
Hello ST Community,I'm encountering difficulties while attempting to connect and debug my STM32 microcontroller, and I'm seeking guidance from the community. I have erased the full chip flash memory and uploaded my code but suddenly I start getting t...
I encountered this error when I was trying to flash my custom board with fresh stm32F070C6T6. I used st link v2 for debugging. I updated the firmware of st link v2 right before debugging. NRST floating, BOOT0 connected to 3V3 -> failed (in any mode)N...
Hi, According to mb1363 for the H755 Nucleo, in order to change from the default SMPS to internal LDO supply, to enable 480 MHz clock, I need to change C54/C58 from 100 nF to 2.2 uF. However it appears that there are no capacitors installed on my boa...
I am unable to obtain ADC values and would like some advice.Here is the source code project.https://github.com/katsumat/STM32CubeIDE/tree/main/workspace_1.16.1/ADCCalibration PA0 is connected to GND, PA1 to Vdd, and PA3 to the output of a variable re...
When I tried to compile a new project using the latest firmware lib function (in keil MDK-ARM uVision), I got these warnings:whether compiling my own project or the template project.It seems like stm32f4xx.h has a lot of incompatible redefinitions? H...
OS: Kubuntu Linux 24.04IDE: STM32CubeIDE 1.17.0 Hello,STM32CubeIDE shows the message "No ST-LINK detected!". Neither the command "lsusb" nor VirtualBox are showing the device. I tried different cables and different USB ports. The quick start guide (U...
Hi,I am currently working on a project using the NUCLEO-H755ZI-Q development board.I am testing with a simple program that turns on the green led and goes to a while loop. I start with "full chip erase" then flash my testing program to the M7 core. I...
I have a a few questions. #1 - Can the STM32H747XI on the STM32H747I-DISCO board be put into a DFU mode?#2 - I have a test app where after it is booted, you can push the WAKE button on the board. The handler for that will then set a magic pattern int...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.