Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L0x Offset calibration and Crosstalk calibration

Hi    follow  can  make offset calibration?Place the object 14cm away .Must be in a dark environment?     follow can make Crosstalk calibration?   Place the object 60cm away. my coverglass like follow,The measured distance seems very short. How can...

zhy_0-1761292891871.png zhy_1-1761293001860.png zhy_2-1761293212141.png zhy_3-1761293684788.png
zhy by Associate III
  • 2148 Views
  • 14 replies
  • 0 kudos

IIO-based Linux driver for VL53L7CH

 Hi, we would like to use the VL53L7CH on Linux 6.12.Standard kernel interfaces are required:IIO/hwmon subsystems and regmap — no proprietary ioctl/miscdevice interface.Is an IIO-based driver for the VL53L7CH already provided or planned for upstream/...

VL6180X IEC 60825-1 CB test certificate

Hello ST:       VL6180X has been discontinued, but our older equipment still uses it. We hope to obtain the IEC 60825-1 CB test certificate to prove its Class 1 rating. However, this certificate is not available on ST's official website, whereas it i...

vl53l4cd variation in readings

Hi, We have incorporated a vl53l4cd into our product. We wish to measure 0 to 100mm with a resolution of 1mm, and an update rate of at most 1 second.We have set the vl53l4cd 19mm back from front measurement face (so we need to actually measure 19 to ...

Resolved! vl53l0x in continue and Time mode

Hi,        vl53l0x in continue mode ,how to read data_status and in time mode how to set time and read data and data_status?               thanks

zhy by Associate III
  • 870 Views
  • 4 replies
  • 0 kudos

Resolved! VL53L0x

 Hi, the rear background exceeds 2 meters, and there are no obstacles in front of the sensor. The measurement data is unstable, and the reading sometimes reaches 0 and sometimes reaches 115.      

zhy_0-1761185641250.png zhy_1-1761186162004.png
zhy by Associate III
  • 3809 Views
  • 2 replies
  • 0 kudos

Reading measurement on VL6180X

STMicroelectronics support,I am testing a VL6180X laser sensor device for use in autonomous robotics.I currently get good distance measurements using an Arduino sketch but can't use that platform in my final product.Instead I'm using a pic18f46k22 mi...

jerryD by Associate
  • 674 Views
  • 1 replies
  • 0 kudos

VL53L8CX RUNNING SPD

Hello, I have a problem when I try to run the SPD code under STM32cube IDE, I have this under the serial monitor which remains stuck like this: SPD ULD SW Kit version 1.0.0Module type = VL53L8CXModule ID : 0000000000000000_VL53L8CBV0GC/1$2FW Version ...

Freedy by Associate II
  • 911 Views
  • 1 replies
  • 0 kudos

Resolved! vd66gy with Raspberry Pi5: Failed to Queue Buffer

I am using a pcb4188_vd66g1 camera module with a Raspberry Pi 5.The system has been freshly set up with Raspberry Pi OS 64-bit, and I followed the official setup guide step by step.After completing the setup:The camera is detected correctly when runn...

05_rpicam-hello--list-cameras.png 06_rpicam-hello_error.png 07_v4l2-ctl--list-devices.png 08_i2cdetect.png
Erebos by Associate
  • 1041 Views
  • 2 replies
  • 0 kudos

Voltage drop when measuring with VL53L0X

Hi everyone,I’m working with the VL53L0X sensor and I noticed that when it starts ranging, the supply voltage (of my board with the VL53L0X, the Vcc pin) drops from 3.389 V down to 2.544 V.In this setup, the VL53L0X is powered from the 3.3 V pin of a...