Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Self test for vl53l8cxv0gc/1

Hi,Currently, we are testing vl53l8cxv0gc/1 by placing an object in front and moving it and reading the values. Is there a way to test the functionality of vl53l8cxv0gc/1 in a production environment? Is there a self test mechanism for this sensor?Tha...

VL53L7CX Motion power

Hi, I'm trying the VL53L7CX sensor for a prototype and I'm trying the example codes provided within  this page https://www.st.com/en/embedded-software/stsw-img036.html I'm experimenting the Example_10_motion_indicator and I'm able to display the "mot...

LudovicB by Associate
  • 873 Views
  • 2 replies
  • 1 kudos

Error in VL53L1X datasheet

On page 9 of https://www.st.com/resource/en/datasheet/vl53l1x.pdf, it is written:"Ranging is continuous, with a programmable delay between two ranging operations (called anintermeasurement period)"This is wrong. It should be:"Ranging is continuous, w...

paul19 by Associate III
  • 675 Views
  • 3 replies
  • 0 kudos

Resolved! VD66GY with IMX8M Mini

Hello ST Brightsense Team,Would like to know if the VD66GY Linux driver (STSW-IMG503_V4L2) will work on an NXP IMX8M Mini (no hardware ISP) ?  If not will it work with the IMX8M Mini Plus (with Hardware ISP).Currently using the STEVAL-66GYMAI.In the ...

FB__1 by Associate III
  • 813 Views
  • 4 replies
  • 0 kudos

Resolved! vl53l8cx_def.h File

Hello,   I am having a hard time finding which software pack this file vl53l8cx_def.h is in? I think once I get that I should be get the zones if Im understanding the error correctly. Please advise.  If it helps with the solution I am trying to use t...

Rhagg28_0-1759612867921.png
Rhagg28 by Associate II
  • 952 Views
  • 4 replies
  • 0 kudos

Resolved! VL53L8 firmware loading

I need to cut off all the power supplys of VL53L8 to save power. Does the firmware need to be re-downloaded every time the device is powered on? loading firmware is in the function uint8_t vl53lmz_init( VL53LMZ_Configuration *p_dev)​

Resolved! Does the noise affect measurements on VL53L0X?

Hi everyone,I'm working with the VL53L0X sensor and have a couple of questions:Does noise affect the sensor's measurements? Does the sensor include a checksum or mechanism to verify the integrity of I2C messages? Can adding capacitors to the I2C bus ...