Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Source available for STSW-IMG041 Device Code ?

Hi,I would like to know if the STSW-IMG041 code that is flashed into the device is available somewhere. My goal would be to use the same code but on a custom board to verify that the sensor is working properly.Thank you! 

MikeReg by Associate II
  • 647 Views
  • 2 replies
  • 0 kudos

Resolved! NUCLEO C09RC-B03 and X-Nucleo 53lxA1

Hello everyone, I would like to know if someone has ever tried to couple those two hardware components together?I am currently using the STM32C092RC board to build an FD-CAN network, and I would like to exchange some real data — or more explicitly, t...

kgb by Associate III
  • 455 Views
  • 1 replies
  • 0 kudos

VL53L7CHV0GC driver not working properly

Hi everyone,I’m having issues with the VL53L7CHV0GC ToF sensor drivers on Linux. The kernel module loads fine, but I can’t read any data using the userspace part. When I try to use the driver completely in userspace mode, it reports that it can’t fin...

nnenadic by Associate II
  • 1049 Views
  • 6 replies
  • 1 kudos

Resolved! Choice of ToF VL53

Hi All, I've been using the VL53L1 sensor for drone height control, and the results have been quite good- however, the environment it is used in has plastic skylights with poor IR blocking. This causes unstable readings in direct sunlight. Some of th...

DM575 by Associate
  • 633 Views
  • 1 replies
  • 0 kudos

VD6283TX45/1

Hello, I am using the VD6283TX45/1 to develop a device and now have a question to consult. Due to my insufficiently careful reading of the data sheet during the initial design phase, I connected the I2C pins of this device to an I2C bus where the pul...

FHL by Associate
  • 483 Views
  • 0 replies
  • 0 kudos

VL53L4CD emitted optical power value

Has anyone seen documentation or done optical power measurements for VL53L4CD? I’m trying to find the radiant energy or optical power output of this low power time-of-flight device. (I only succeed to find a graph showing the relative emitted power i...

VL53L4CD_Relative Emmited Power.png
ali_Kiwi by Associate
  • 607 Views
  • 1 replies
  • 0 kudos